Part Number: TM4C123GH6PM
Tool/software: Code Composer Studio
Hi,
I have a sd connected by spi to uC, I use the USB as Mass Storage Device so that when connected to a host (PC) can read the sd. I can not understand which role meets the variable usMAXPowermA (energy consumption) if for example in my case the power is taking from uC. What does the maximum consumption mean if the uC does not deliver more than a few mA? Usually set to (500mA).
Of course, the ucPwrAttributes variable is set to Self Powered.
Thanks and Regards!
Alberto.-