This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294NCPDT: TM4C1294NCPDT and TM4C129ENCPDT compatability

Part Number: TM4C1294NCPDT


Currently we use a TM4C1294NCPDT but we are having availability problems. I looked at the drop-in selection and the only alternative with same footprint, flash, MAC and PHY is the TM4C129ENCPDT. The only difference is the E version has a HW accelerator for encryption. Since it seems more widely available, we are considering approving it as an alternate. Our question boils down to this: we want to avoid a time consuming re-vetting process to qualify this part, so we’d like to know if this can be dropped into our current design without  risk. I figure since our current design does not use the feature, there should be no issues, but wanted some confirmation from an official source that knows the risk.

Any help would be appreciated.

Cheers

Calum

  • Hi Calum,

      You are correct the only difference is the hw security accelerator. As long as you don't use them there is no compatibility issue. 

      TM4C1294NCPDT TM4C129ENCPDT
       
    Order now Order now
    Online datasheet Online datasheet
    Datasheet Datasheet
    Tools & Software Tools & Software
       
    CPU ARM Cortex-M4F ARM Cortex-M4F
    Pin & Package 128TQFP 128TQFP
    Flash (KB ) 1024 1024
    SRAM (kB ) 256 256
    Max Speed (MHz) 120 120
    Motion PWM Outputs 8 8
    QEI 1 1
    GPIO 90 90
    Operating Temperature Range (C ) -40 to 105 -40 to 105
    -40 to 85 -40 to 85
    USB D, H/D, or OTG OTG OTG
    SSI/SPI 4 4
    I2C 10 10
    UART 8 8
    ADC Channels 20 20
    ADC Resolution (Bits ) 12 12
    CAN MAC 2 2
    SysTick Yes Yes
    Security No HW accelerator HW accelerator
    External Peripheral Interface Yes Yes
    10/100 ENET MAC+PHY Yes Yes
    USB High-Speed with ULPI Yes Yes
    10/100 ENET MAC No No
    LCD Controller No No
    1-Wire Master 0 0
    Bi- and Quad- SSI/SPI Yes Yes
    Package Size: mm2:W x L (PKG) 128TQFP: 256 mm2: 16 x 16(TQFP) 128TQFP: 256 mm2: 16 x 16(TQFP)
    Frequency (MHz ) 120 120
    Non-volatile Memory (KB) 6 6
    Package Group TQFP TQFP
    RAM (KB ) 256 256
    Rating Catalog Catalog
    Approx. Price (US$) 8.07 | 1ku 8.66 | 1ku
    SPI 4 4