This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294KCPDT: The schematic of XDS200's adapter

Part Number: TM4C1294KCPDT


Hi,

I use XDS200 USB Debug Probe-TMDSEMU200-U and the adapter that converts TI 20-pin to ARM 20-pin, to connect TM4C1294(the TMS,TCK,TDO,TDI,RST,VCC,GND pin). But rencently I lost this 20-pin to 20-pin adapter, so I want to know the schematic of this adapter and connect XDS200 to TM4C1294 by myself, can you provide it? I know there are some resistor and a switch on this adapter, but I do not know their function and which pin they connects to. If it is convenient, please offer  the  schematic of 20-pin to 20-pin adapter, thanks!

  • Hi Shaw,
    Please refer to this wiki page for more information on the pin mapping. 

  • Interestingly, I lost my ARM 20-pin to ARM-10 pin adapter... Rather, not lost it, but "ripped it off a board".

    So if the schematics are available for that board as well, that's welcome!

    And for the one you need, as a bit of recreational pause, I was able to get the following basics:

    Hope this does not infringe any copyright - I'll immediately remove the post if that's the case...