Part Number: TM4C129ENCPDT
Other Parts Discussed in Thread: UNIFLASH, EK-TM4C1294XL, TM4C1294NCPDT, TM4C123GH6PM
Hi,
I have a new TM4C129ENCPDT processor, to which I successfully flashed the blinky code via UART0 using LM Flash Programmer utility.
Now, I want to again flash a new code, but I am facing an error reprogramming the code using LM Flash (error is : Failed to synchronize Baud rate ). I think that the problem is that: for the first time, when I was flashing blinky code, ROM bootloader was invoked (it checked for location 0x04 and it was empty) and the code was flashed using UART0 . But now there is already something present in the flash, due to which ROM bootloader is not working, hence baud rate is not synchronized.
So every time, I want to flash the code using UART0 via ROM bootloader, I will have to erase flash, but I am unable to find any utility to do it.
I tried UNIFLASH, but the board is not getting recognised.