Part Number: TMS470R1B1M
Hi all,
I'm having issues programming a TMS470R1B1M
I have four identical boards each withthe same microcontroller and batch code CA-41C91W. One programmes without a problem the other 3 fail with the same error "CPU-failed to stop".
I have checked the cloack 7.5MHz, 1.8V is good 3.3Volts is good.
Jtag data is going to and from the uP
Osc out is also working
TRSTn is pulled low with 10k
RTclk is pulled low with 10k
RSTn is pulled high with 10k
There is nothing else on the Jtag bus
The IAR software log is as follows
Tue Sep 26, 2017 16:17:36: IAR Embedded Workbench 8.11.1 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\bin\armproc.dll)
Tue Sep 26, 2017 16:17:36: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\config\flashloader\TexasInstruments\FlashTMS470R1B1M.mac
Tue Sep 26, 2017 16:17:36: Loading the I-jet/JTAGjet driver
Tue Sep 26, 2017 16:17:36: Probe: Probe SW module ver 1.59
Tue Sep 26, 2017 16:17:36: Probe: Option: trace(Auto,size_limit=100%)
Tue Sep 26, 2017 16:17:36: Probe: I-jet-Trace SW module ver 1.63
Tue Sep 26, 2017 16:17:36: Probe: Found I-jet, SN=82752
Tue Sep 26, 2017 16:17:36: Probe: Opened connection to I-jet:82752
Tue Sep 26, 2017 16:17:36: Probe: USB connection verified (10181 packets/sec)
Tue Sep 26, 2017 16:17:36: Probe: I-jet, FW ver 4.2, HW Ver:A
Tue Sep 26, 2017 16:17:37: Probe: IJET-ARM20 adapter detected
Tue Sep 26, 2017 16:17:37: Probe: Versions: JTAG=1.78 SWO=1.37 A2D=1.70 Stream=1.48 SigCom=2.43
Tue Sep 26, 2017 16:17:37: Emulation layer version 4.17
Tue Sep 26, 2017 16:17:37: JTAG clock detected: 12MHz
Tue Sep 26, 2017 16:17:37: Notification to init-after-power-up hookup.
Tue Sep 26, 2017 16:17:37: Notification to core-connect hookup.
Tue Sep 26, 2017 16:17:37: CPU status OK
Tue Sep 26, 2017 16:17:37: LowLevelReset(software, delay 200)
Tue Sep 26, 2017 16:17:40: Fatal error: CPU did not stop Session aborted!
Tue Sep 26, 2017 16:17:40: Unloaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\config\flashloader\TexasInstruments\FlashTMS470R1B1M.mac
Tue Sep 26, 2017 16:17:41: IAR Embedded Workbench 8.11.1 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\bin\armproc.dll)
Tue Sep 26, 2017 16:17:41: Loading the I-jet/JTAGjet driver
Any suggestions I'm a bit stuck having not used TI processors before?
many thanks in advance..