Part Number: TMS570LS0232
Other Parts Discussed in Thread: HALCOGEN,
Tool/software: Code Composer Studio
Hello,
We use the HALCoGen configuration, Flash configuration options cannot be found aside. We are using the HALCoGen default configuration, and the Flash has an error code "#10099-D program will not fit into available memory. Placement with alignment fails for section ".cinit" size 0x461. Available memory ranges: sys_link.cmd /TMS570LS0232/source line 79 C/C++ Problem"
When we manually configure the Flash to the maximum, is not wrong. We use the HALCoGen automatic configuration after the generated code, and then manually configure the maximum Flash.Is this operation compliant?
If Flash is not enough, the compiled HEX file has the largest 79KB, and this error occurs. The maximum Flash of TMS570LS0232 is 128KB.. What's the problem with configuring CCS?