This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: Pin & Ports of TMS570LC43x

Part Number: TMS570LC4357


Hello,

i have a little problem with understanding the Port and Pins of this board.

Do i have 'Ports' on this Board? Or is every Module like ADC a own Port.

For Example i have 32 Pins :

How can i access to those Pins ? On my board there are names like J10 J9 and so on.

I Know that Pin 6 is my Temp Sensor on the board, because i have read it directly from the board. But for example i want to enable Pin 2. Where can i connect my sensor on?

Thank you