Other Parts Discussed in Thread: TPS65381A-Q1
Hello,
I have some questions about output pin indication of internal watchdog trip.
The datasheet lists two pins that can used for this, nRST and nERROR. Which pin is the best pin to use for output indication of internal watchdog trip? What are the pros and cons for each pin used for this?
When an internal watchdog trips, do both nRST and nERROR stay low after they are driven low, or do they only go low for some minimum pulse width? We need it to stay low until we set it high again.
If they stay low for watchdog trip, what is needed to get either of them to go logic high again?
Datasheet seems to indicate that nRST is also driven low for reset conditions. Is this also the case for nERROR? Can you point me to where it says this?
Besides reset, if we only want the pin to go low for watchdog trip, is there a way to configure this, or are there several other fixed conditions that will cause nRST or nERROR to go low? Datasheet table 6-5 for nRST and table 6-35 for nERROR seem to indicate there a several fixed conditions that will cause either nRST or nERROR to be driven low and cannot be configured otherwise. Am I interpreting this correctly?
Would we be better off to just use a GPIO output to indicate only a watchdog trip as well as reset condition. If so how would this be best implemented using a GPIO to do this?
Thanks,
Scott