Part Number: TMS570LS0232
Tool/software: Code Composer Studio
Hi
I have some questions to ask about using TMS570LS0232
1.on the Flash question, whether you can provide Flash drivers, and the location of Flash is locked, the customer asked whether you can customize the location, specify the location of writing bootload, to avoid each upgrade position changes.
2. I want to save space, does not compile the sys_pcc.c and sys_selfttest.c files, I want to separate configuration involves functional safety inspection, it can optimize a lot of space, you can through the self configuration of functional safety certification.
3. About the configuration of RTI, I would like to use Compare to do some timing work without interrupting
4.On the ESM configuration, whether you can configure Group2 and 3 configuration, as well as Group1 can also output nError signal, ESM interrupt is every regular inspection or running test procedures to run
5.About the configuration of CRC, whether it can not be enabled?
6.Now the generated hex file size does not exceed the size of flash, but the display in the map file size is beyond the size of Flash, if you use other compiler if you get a different size, which is good
7.I want to optimize the program flash space, and what's the best possible space solution in CCS, thank you