Part Number: TM4C123GH6PGE
Other Parts Discussed in Thread: EK-TM4C1294XL
Hello,
I got the below code from one of the previous answer in the forum.Now i want to set the starting time from today like 11 october 2017 and start the time from present time like 18:05:26, anyone please tell me how to set above values in my below code
// Global data to be used by this example
//
//*****************************************************************************
time_t calendar_write;
time_t calendar_read;
struct tm tm1 = {50,59,23,5,6,2014-1900,5,0,0}; // to compute seconds since epoch
struct tm tm2 = {0}; // to read back the calendar
uint8_t buf_er[] = "Wrong initialization structure!\n";
uint8_t buf_rz[48];
void UARTSend(uint8_t *pui8Buffer, uint32_t ui32Count);
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
//*****************************************************************************
//
// Hibernate handler
//
//*****************************************************************************
void HibernateHandler(void)
{
// reset interrupt flag
uint32_t ui32Status = HibernateIntStatus(1);
ROM_HibernateIntClear(ui32Status);
//
calendar_read = HibernateRTCGet();
ulocaltime(calendar_read, &tm2);
// format the output for uart
strftime((char *)buf_rz, 32, "%c\r\n", &tm2);
UARTSend((uint8_t *)buf_rz, 32);
// Keep the interrupt hapening
HibernateRTCMatchSet(0,HibernateRTCGet()+5);
}
//*****************************************************************************
//
// Send a string to the UART.
//
//*****************************************************************************
void
UARTSend(uint8_t *pui8Buffer, uint32_t ui32Count)
{
//
// Loop while there are more characters to send.
//
while(ui32Count--)
{
//
// Write the next character to the UART.
//
ROM_UARTCharPut(UART0_BASE, *pui8Buffer++);
}
}
int main(void) {
//
// Enable lazy stacking for interrupt handlers. This allows floating-point
// instructions to be used within interrupt handlers, but at the expense of
// extra stack usage.
//
ROM_FPUEnable();
ROM_FPULazyStackingEnable();
//
// Set the clocking to run directly from the crystal.
//
ROM_SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);
//
// Enable the GPIO port that is used for the on-board LED.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
//
// Enable the GPIO pins for the LED (PF2).
//
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_2);
//
// Enable the peripherals used by this example.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Enable processor interrupts.
//
ROM_IntMasterEnable();
//
// Set GPIO A0 and A1 as UART pins.
//
ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Configure the UART for 115,200, 8-N-1 operation.
//
ROM_UARTConfigSetExpClk(UART0_BASE, ROM_SysCtlClockGet(), 115200,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));
//
// Configure the hibernation module
//
ROM_HibernateEnableExpClk(0);
ROM_HibernateRTCEnable();
HibernateClockConfig(HIBERNATE_OSC_HIGHDRIVE);
//
HibernateIntRegister(HibernateHandler);
HibernateIntEnable(HIBERNATE_INT_RTC_MATCH_0);
HibernateWakeSet(HIBERNATE_WAKE_RTC);
//Set up counter mode for RTC
HibernateCounterMode(HIBERNATE_COUNTER_RTC);
//
// Calculate the calendar data to be written
//
calendar_write = umktime(&tm1);
if (calendar_write == (uint32_t)(-1)){
UARTSend((uint8_t *)buf_er, sizeof(buf_er));
while(1);
}
else {
HibernateRTCSet(calendar_write);
//Set an interrupt for the RTC after one second.
HibernateRTCMatchSet(0,HibernateRTCGet()+5);
}
while(1){
//do nothing - safety
}
// return 0;
}
Thanks in advance.