Part Number: EK-TM4C123GXL
The CircuitCo Audio Boosterpack for the TM4C123 Launchpad that is referred to in the book 'Digital Signal Processing using the ARM Cortex-M4'
never went into full-scale production.
I have just requested the addition of materials to the companion website for the book that include schematics, BOM, and gerber files for an
alternative audio boosterpack. I hope they'll appear very soon.
As shown in images contained in the materials (and below), I have constructed that boosterpack. It is a relatively simple pcb - two-sided, no
plated-through holes - and the components were soldered by hand. This is quite fiddly but self-evidently possible. The most difficult
component to solder is the codec. The pcb tracks are such that either a Texas Instruments AIC23 or a Cirrus Logic WM8731 codec
may be used. The packages that I could find were slightly different widths. In 28-pin SSOP packages only two pin functions are swapped but this has no bearing on the device's use
in this Boosterpack.
If you construct your own Boosterpack from the design given then you can use it with the book pretty much seamlessly. The biggest
difference between the new Boosterpack (AIC23/WM8731 codec) and the CircuitCo Boosterpack (AIC3104 codec) referred to explicitly
in the book is that the AIC23 doesn't contain configurable IIR filters (biquads) and so the program examples concerning these have no
equivalents that will run with the new Boosterpack.
The book can also be used (program examples are on the companion website) with the Cypress Semiconductor FM4 S6E2CC pioneer
hardware platform which uses the same WM8731 codec as the new audio boosterpack.