Part Number: TM4C1294NCPDT
Tool/software: Code Composer Studio
Hello,
I'm working on a project where one TM4C1294NCPDT needs to load a firmware to another one through SSI. The problem is that it seems like there is already a program inside the target MCU, which somehow doesn't allow reprogramming via SSI.
Aggravating circumstances: both are inside a PCB. The "loader" MCU has external JTAG connection, which is where it is programmed from. Now, the target MCU has only an SSI connection to the first, no more. They're all extremely hard to solder SMDs. So, jumper connections to any pin will be almost impossible in my lab.
Question: Can the loader MCU erases all target's memory or forces the code to be written through SSI? If not, is there any way I can do that, considering circumstances?
Thanks,
Nori