Part Number: TMS570LS1115
Tool/software: Code Composer Studio
Hi everyone,
I'm trying to optimize system efficiency by implementing ADC+DMA data transfer, which was using FIFO before.
Testing HW Circuit Board is well developed, which means it's very difficult to change any HW architecture or TMS570 Pins definition.
Here a demo project.
With ADC + DMA implemented, which is working fine on our HW Circuit Board.
However, when I trying to integrate this DMA function with our software, it seems DMA never be triggered.
What I trying to do is generating 3 ADC DMA Requests (ADC1 Group1; ADC1 Group2; ADC2 Group1) in three configurable DMA Request lines during a single circle. This may be a configuration issue of DMA Request lines(red line in the figure above), the question is:
- In the project uploaded, ADC was accidentally sent DMA_REQ by DMA Request Line 7 successfully (at least I don't know how to configure this), can anyone give me a hit on how this project configure DMA Request Line 7 to transfer DMA Request from ADC1 Event Group (for example change to Request Line 1)?
- Is there any Register for DMA Request line configuration of Different ADC groups? or is it just possible configured in hardware level?
- In DMA module, there is SW and HW trigger method, does SW trigger will introduce CPU external workload? Does HW trigger method need more free TMS570 PINs in HW level?
Regards,
Jason