Part Number: EK-TM4C129EXL
Other Parts Discussed in Thread: EK-TM4C1294XL
Hi,
I am new to CAN protocol, please forgive me if i am asking a foolish query. I have configured a CAN-0 peripheral of TM4C129-EXL evaluation board and attempt to send a 32 bit hex data. on evaluating the transmitted CAN frame format on DSO, it looks like the data is correct according to the data send. How can i validate the transmitted data by receiving it through another CAN peripheral? (CAN transceiver and CAN bus with 120 ohm termination is already implemented with the same).
- The major query is about CAN-1 signals, i found that the TX signal (PB1) in CAN-1 in TM4C129EXL evaluation board is going to "TARGET_VBUS/3.2C". is there any way that i can use CAN-1 signals in this same evaluation board to validate the transmit signals from CAN-0?, if not possible then what is the solution to validate CAN data receive firmware?
Some help is greatly appreciable, thanks in advance.