Part Number: TM4C1294NCPDT
Hi,
I had to deal with one problem and have just been informed on the other.
1. Upon power-up (autonomos, not via VBUS) in maybe two out of many devices (USB0VBUS pin is configured as USB, not PB1 - I did not write the code) the pin were consistently driven low, loading VBUS (successfully - 5V was going down to under 4V). After unplugging / plugging back the USB cable the USB would start functioning. Eventually the pin was damaged. I remedied this by inserting 1K resistor in series with the pin, and in the spun version also put a 3.6V Zener after it to counter ESD and 5V in case it does something to the pin. So far seems to work.
2. Today we have been made aware that when the device is powered down but the USB Master (our device is used as a slave) is still plugged in, the CPU stays powered. I have not found anything mentioning the CPU could be powered via the USB0VBUS pin (the only connection to any power at that point.)
What gives?
Best, Mike