Part Number: TMDX570LC43HDK
Other Parts Discussed in Thread: HALCOGEN
Hy,
I'm working on a TMDX570LC43HDK board,
I would like to use as much as possible the "Hercules Safety MCU Demos"
regarding this what seems strange to me are the following points:
- when I import the CCS project from "C:\ti\Hercules\Hercules Safety MCU Demos\4.0.0\TMS570LC43x_target_sources" I obtain an almost empty project so I've to fill the folder "Halcogen" and "demo-app" manually, but it is ok, after this I can build the project and deploy it to the board
- Is not available the Halcogen project to import in Halcogen
- When I start the project in debug and then open the labview interface it seems to work fine but it is not, for example the led demo is not working (but I've not a communication error)
- If I reset the board with PORRST i can pilot the demo from the LabView interface but I've no more debug available
- When I click on Code Composer STudio on Labview interfaceit just open CodeComposerStudio
Finally If possible I'm interested to the Halcogen project and in debug the TMDX570LC43HDK C application driven from Labview interface.
Thanks
Antonio