Part Number: RM48L530
Other Parts Discussed in Thread: TPS65381A-Q1
Hi,
I am wondering if there is any requirement for an external watchdog connected to an RM48 (or maybe even any CPU in general) when it comes to the type of reset it should assert.
The TPS65381 uses the power-on reset (cold reset), but this IC also does voltage monitoring, so it could be because of that.
The internal watchdog asserts a warm reset, for which also a flag is set during the reset.
The same can be done using the nRST pin of the CPU, which asserts a warm reset as well.
The benefit of this approach is knowing the reason behind the reset, but I am not sure if this is allowed for functional safety.
I could not find any recommendation regarding the type of reset asserted by an external watchdog in the RM48 safety manual nor in the IEC 61508 standard.
Can you help me with this?
Thank you in advance!