Part Number: TMS570LC4357
Hi,
We are develloping a new system with the TMS570LC4357. The system works fine in room temperature useage. But once we perfome thermal cycling testing (to 85C), the ADC fails. All the inputs gives the same proportional results, that is, for the same voltage, the results is the same. The ADREFHI draws 17mA and lowers the referance (2.8V instead of 3V). We have done the testing on multiples units and all seems to fails the ADC conversion. It is hard to troubleshoot them since they are casted in Nylon.
We are trying to find out what kind of failuer would cause the input of the ADREFHI to fail and draw higher current them the specs expect. All other voltage measured after the thermal cycling are normal and within specs. The only failling voltage is the ADREFHI.
If anyone has a similar issue or got a similare faillure of the ADREFHI, please let me know.
Some more details:
ADREFHI: 3V - REF5030AQDRQ1
ADREFLO: 0V
VCCAD: 3.3V - TPS65381QDAPRQ1
VSSAD: 0 V
One of my hypothesis is if VSSAD falls to 0V and that ADREFHI is still 3V, would the ADREFHI clamp in a short and damage the overvolatge clamps?
Ben