Part Number: TMDX570LC43HDK
Hy,
in our project we need to connect the TMDX570LC43HDK board to 2 sensors having each one an RS422 interface,
How it is possible to connect such devices to this board?
Considering just one sensor it is possible to use the USB/serial/JTAG connector J7,
but how to connect two different sensors?
Could be useful the second JTAG Connector J4?
This is just a connector for an external JTAG debugger by my point of view,
it could be used to debug a board that already use the USB connector for a SCI,
is this right?
Please excuse me but I've a little bit of confusion about these points.
Thanks
Antonio