Part Number: TMS570LS3137
Hello,
I'm reposting an issue that one of my colleagues posted back in July that we have not resolved yet.
Link to his post: https://e2e.ti.com/support/microcontrollers/hercules/f/312/t/612079
In general we are using HET pin 30 to capture a 32Khz signal 3vpp and then using pin 31 to output a High if the signal exceeds the 32Khz. We are seeing very erratic results (meaning pin 31 does not always go high right at 32Khz) based on small changes in the input frequency amplitude.
Even with the amplitude staying the same, after a reset to the MCU, the trigger point is not always detected.
We have both pins configured with pull-down resistors for code generation.
Any suggestions or feedback would be greatly appreciated.