This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL2-RM57L: Embedded Coder problem

Part Number: LAUNCHXL2-RM57L

Hy,

I'm trying to deply the "arm_cortex_r_gettingstarted" symulink model to -the LAUNCHXL2-RM57L board

accorfing to this tutorial:

www.mathworks.com/.../armcortexr_product-arm_cortex_r_gettingstarted-getting-started-with-embedded-coder-support-package-for-arm-cortex-r-processors

but the result is the following error log:

C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_sys_link.cmd <Linking> undefined first referenced symbol in file --------- ---------------- MPU_xTimerCreate mw_timer.obj xQueueCreateCountingSemaphoreStatic os_mpu_wrappers.obj xQueueCreateMutexStatic os_mpu_wrappers.obj xTimerPendFunctionCall os_mpu_wrappers.obj error #10234-D: unresolved symbols remain error #10010: errors encountered during linking; "../arm_cortex_r_gettingstarted.out" not built >> Compilation failure gmake: *** [../arm_cortex_r_gettingstarted.out] Error 1 C:\prj\Matlab\arm_cortex_r_gettingstarted_ert_rtw>echo The make command returned an error of 2 The make command returned an error of 2 C:\prj\Matlab\arm_cortex_r_gettingstarted_ert_rtw>An_error_occurred_during_the_call_to_make 'An_error_occurred_during_the_call_to_make' is not recognized as an internal or external command, operable program or batch file.

how can I solve the problem that seems common also to other examples.

Thanks

Antonio

----

This is the full log:

---------

arm_cortex_r_gettingstarted
 Build  4  2  1 Clear
09:46 PM Elapsed: 0.122 sec
### Starting build procedure for model: arm_cortex_r_gettingstarted
### Generating code and artifacts to 'Model specific' folder structure
 Code Generation  2  2
Elapsed: 57 sec
### Generating code into build folder: C:\prj\Matlab\arm_cortex_r_gettingstarted_ert_rtw
All blocks in block diagram 'arm_cortex_r_gettingstarted' are either virtual or have been removed by block reduction optimization or they are inactive variants, therefore there is nothing to simulate. Note, for code generation, block reduction optimization removes all diagram branches terminating in sink blocks that do not participate in code generation. For example, To Workspace blocks and potentially their sources are removed when the MAT-file logging is off
Component:Simulink | Category:Block diagram warning
Code generation objectives not specified for 'arm_cortex_r_gettingstarted'.
  Suggested Actions
 Specify objectives
Open
Set 'Check model before generating code' to 'Off'
Open
Component:Simulink | Category:Block diagram warning
### Invoking Target Language Compiler on arm_cortex_r_gettingstarted.rtw
### Using System Target File: C:\Program Files\MATLAB\R2017b\rtw\c\ert\ert.tlc
### Loading TLC function libraries
### Initial pass through model to cache user defined code
.
### Caching model source code
### Writing header file arm_cortex_r_gettingstarted_types.h
### Writing header file arm_cortex_r_gettingstarted.h
.
### Writing header file rtwtypes.h
### Writing source file arm_cortex_r_gettingstarted.c
### Writing header file arm_cortex_r_gettingstarted_private.h
### Writing header file rtmodel.h
### Writing source file ert_main.c
### TLC code generation complete.
.### Evaluating PostCodeGenCommand specified in the model
### Using toolchain: TI ARM Code Generation Tools | gmake
### 'C:\prj\Matlab\arm_cortex_r_gettingstarted_ert_rtw\arm_cortex_r_gettingstarted.mk' is up to date
### Building 'arm_cortex_r_gettingstarted': "C:\PROGRA~1\MATLAB\R2017b\bin\win64\gmake"  -f arm_cortex_r_gettingstarted.mk all
C:\prj\Matlab\arm_cortex_r_gettingstarted_ert_rtw>cd .
C:\prj\Matlab\arm_cortex_r_gettingstarted_ert_rtw>if "" == "" ("C:\PROGRA~1\MATLAB\R2017b\bin\win64\gmake"  -f arm_cortex_r_gettingstarted.mk all )  else ("C:\PROGRA~1\MATLAB\R2017b\bin\win64\gmake"  -f arm_cortex_r_gettingstarted.mk  )
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="arm_cortex_r_gettingstarted.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=arm_cortex_r_gettingstarted.obj arm_cortex_r_gettingstarted.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="HL_epc.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=HL_epc.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_epc.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="HL_errata.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=HL_errata.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_errata.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="HL_esm.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=HL_esm.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_esm.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="HL_nmpu.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=HL_nmpu.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_nmpu.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="HL_notification.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=HL_notification.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_notification.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="HL_pinmux.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=HL_pinmux.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_pinmux.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="HL_sys_dma.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=HL_sys_dma.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_sys_dma.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="HL_sys_pcr.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=HL_sys_pcr.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_sys_pcr.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="HL_sys_phantom.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=HL_sys_phantom.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_sys_phantom.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="HL_sys_pmm.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=HL_sys_pmm.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_sys_pmm.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="HL_sys_startup.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=HL_sys_startup.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_sys_startup.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="HL_sys_vim.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=HL_sys_vim.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_sys_vim.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="HL_system.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=HL_system.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_system.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="os_croutine.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=os_croutine.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/os_croutine.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="os_event_groups.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=os_event_groups.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/os_event_groups.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="os_heap.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=os_heap.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/os_heap.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="os_list.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=os_list.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/os_list.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="os_mpu_wrappers.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=os_mpu_wrappers.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/os_mpu_wrappers.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="os_port.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=os_port.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/os_port.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="os_queue.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=os_queue.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/os_queue.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="os_tasks.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=os_tasks.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/os_tasks.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="os_timer.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=os_timer.obj C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/os_timer.c
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl -s -ml -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_sys_core.asm
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl -s -ml -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_sys_intvecs.asm
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl -s -ml -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_sys_mpu.asm
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl -s -ml -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_sys_pmu.asm
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl -s -ml -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/os_portasm.asm
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --compile_only -i"C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/include" --preproc_with_compile --preproc_dependency="ert_main.pp" --obj_directory="./" -g -mv7R5 --code_state=32 --float_support=VFPv3D16 --abi=eabi -me --diag_wrap=off --display_error_number --diag_warning=225 --enum_type=packed -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DEXTMODE_DISABLEPRINTF -DUSE_FREERTOS -DSTACK_SIZE=64 -DRT -DOS_TICK=200 -DOS_STKSIZE=1088 -DINCLUDE_xTaskGetCurrentTaskHandle=1 -DOS_CLOCK=75000000 -DMODEL=arm_cortex_r_gettingstarted -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/prj/Matlab -IC:/PROGRA~1/MATLAB/R2017b/simulink/include/sf_runtime -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/serial -Iinclude -IC:/prj/Matlab/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tirm57lx/include -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/freertos/include -IC:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/include --output_file=ert_main.obj ert_main.c
"### Creating standalone executable "../arm_cortex_r_gettingstarted.out" ..."
C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/bin/armcl --run_linker --rom_model --search_path=C:/ti/ccsv6/tools/compiler/ARM_15~1.LTS/lib -mv7R5 -me -m"arm_cortex_r_gettingstarted.map" --warn_sections --reread_libs --diag_wrap=off --display_error_number --diag_warning=225 --xml_link_info="arm_cortex_r_gettingstarted_linkInfo.xml" --rom_model --heap_size=0x5000 --stack_size=0x1000 --output_file=../arm_cortex_r_gettingstarted.out arm_cortex_r_gettingstarted.obj TI_RM57Lx_init.obj mw_freertos_init.obj mw_thread.obj mw_timer.obj mw_semaphore.obj HL_epc.obj HL_errata.obj HL_esm.obj HL_nmpu.obj HL_notification.obj HL_pinmux.obj HL_sys_dma.obj HL_sys_pcr.obj HL_sys_phantom.obj HL_sys_pmm.obj HL_sys_startup.obj HL_sys_vim.obj HL_system.obj os_croutine.obj os_event_groups.obj os_heap.obj os_list.obj os_mpu_wrappers.obj os_port.obj os_queue.obj os_tasks.obj os_timer.obj HL_sys_core.obj HL_sys_intvecs.obj HL_sys_mpu.obj HL_sys_pmu.obj os_portasm.obj ert_main.obj C:/ti/ccsv6/tools/compiler/arm_15.12.3.LTS/lib/rtsv7R4_T_le_v3D16_eabi.lib C:/prj/Matlab/arm_cortex_r_gettingstarted_ert_rtw/source/HL_sys_link.cmd
<Linking>
 undefined                           first referenced
  symbol                                 in file
 ---------                           ----------------
 MPU_xTimerCreate                    mw_timer.obj
 xQueueCreateCountingSemaphoreStatic os_mpu_wrappers.obj
 xQueueCreateMutexStatic             os_mpu_wrappers.obj
 xTimerPendFunctionCall              os_mpu_wrappers.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking;
   "../arm_cortex_r_gettingstarted.out" not built
 
>> Compilation failure
gmake: *** [../arm_cortex_r_gettingstarted.out] Error 1
C:\prj\Matlab\arm_cortex_r_gettingstarted_ert_rtw>echo The make command returned an error of 2
The make command returned an error of 2
C:\prj\Matlab\arm_cortex_r_gettingstarted_ert_rtw>An_error_occurred_during_the_call_to_make
'An_error_occurred_during_the_call_to_make' is not recognized as an internal or external command,
operable program or batch file.
### Creating HTML report file arm_cortex_r_gettingstarted_codegen_rpt.html
### Build procedure for model: 'arm_cortex_r_gettingstarted' aborted due to an error.
Error(s) encountered while building "arm_cortex_r_gettingstarted":
### Failed to generate all binary outputs.
Component:Simulink | Category:Block diagram error