Part Number: LAUNCHXL2-RM57L
Other Parts Discussed in Thread: HALCOGEN, LM324
Hi,
I have the version of the pcb hercules Launch XL2-RM57 (B) Rev (A1).
I am using 3 channels AD1 [0], AD1 [7] and AD1 [18]. In ADC1_0 I am entering a triangular signal of 50hz, by ADC1_7 I am entering a sinusoidal signal of 50Hz and by ADC1_18 I am entering a continuous signal of 2V.
The result of the ADC channels is a mixture of the 3 signals.
I Check that by entering only one signal and measuring with an oscilloscope on the input pins of the other two ADCs, I can see the entered signal on the oscilloscope screen.
As if the pins of the ADCs were electrically connected.
Thanks for your help .
Best regards
Diego Elisei