Part Number: TM4C123GH6PM
Hello !
I have successfully implemented filter in KEil using cmsis dsplib.
Now, i am trying to implement fast rfft for 1024 real data.
I was able to successfully run example given for cfft in keil.
With this same project settings,I modified code to implement 1024 real fft. When i compiled code,it gives following error
.\ARMCM0_debug\arm_fft_bin_example.axf: error: L6047U: The size of this image (91344 bytes) exceeds the maximum allowed for this version of the linker
Pl. let me know how to work around this error.
My Main includes following code
arm_rfft_fast_instance_f32 fftInstance;
arm_status status;
float32_t maxValue;
status = arm_rfft_fast_init_f32(&fftInstance,fftSize);
/* Process the data through the rFFT/CIFFT module */
arm_rfft_fast_f32(&fftInstance, testInput_f32_ppg,testOutput,ifftFlag);
/* Process the data through the Complex Magnitude Module for
calculating the magnitude at each bin */
arm_cmplx_mag_f32(testInput_f32_ppg, testOutput, fftSize);
/* Calculates maxValue and returns corresponding BIN value */
arm_max_f32(testOutput, fftSize, &maxValue, &testIndex);
Thanks & Regards,
Neelima