Part Number: TMS570LC4357
Hello,
I'm not able to reproduce the results of the ECC calculation in table 3 (without address) in the following document

For example:
(hex values)
DATA: 954F6D2F2992A9B6 ECC: AA MY ECC: 5A
DATA: 8F8342C3E7DE1D53 ECC: 14 MY ECC: E4
DATA: 554B0A86A8F07BDB ECC: 41 MY ECC: B1
The lower 4 bits of the ECC are correct, the upper 4 bits are inverted for some reason.
I used the table 1 to get which of the 64 data bits must be xor'ed for each ECC bit. After that I made an additional xor with 1 to bits 2 and 3 of the ECC to take into account the odd parity of these bits.
Any ideas? Is there something wrong with the document or am I just missing something ?
Best regards,
Mario