Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDX570LC43HDK: Interaction between FreeRTOS and a 100us interrupt

Part Number: TMDX570LC43HDK
Other Parts Discussed in Thread: HALCOGEN

Hy,

why it is not possible to enable RTI on HalCoGen if I choose to create a FreeRTOS project?

I think it is used for the tick, if this is true it means that I can't create also an interrupt,

for example I need a 100us interrupt interacting with freeRTOS, it is possible to achieve this?

Thanks

Antonio