Other Parts Discussed in Thread: TMS570LS20216
Hello,
In the TRM for TMS570, it is mentioned that CCM can generate ERROR Signal to ESM module in "ERROR Forcing Mode [MKEY=1001]" and "SelfTest Error Forcing Mode[MKEY=1111]".
In the Device Data Sheet for TMS570LS20216 I find the following under section
3 Reset / Abort Sources
Error Source System Mode Error Response ESM Hookup group channel
Self test failure User/Privilege ESM 1.31
Compare failure User/Privilege ESM => NMI 2.2 Now, which one of the above "RESET/ABORT Source" line is linked to MKEY=1001 and which one is for MKEY=1111? I am assuming MKEY=1111 is only for "SELF TEST FAILURE" Line of RESET ABORT Source. MKEY=1001 is only for "Compare Error" Line of RESET ABORT Source and in effect it is NMI. Is the correct? Thank you. Regards Pashan