Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: Resetting DMA control packets immediately after they complete

Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN

I have observed some very strange behavior when resetting (via writing to it) a DMA control packet immediately after it finishes. I have observed this with multiple peripherals so I do not think it is related to which one. Specifically, it seems to put the last element of the transfer where the first one should go and doesn't write anything in the last element's memory location.

A short delay in between observing the DMA peripheral indicating the transfer is done and writing to the control packet makes the symptom go away. However, I do not see any mention of this requirement in the TRM, so I do not know how long a delay guarantees correct behavior (and how it depends on clock speeds etc). Could you clarify the timing requirements around this use case?

The rest of this post summarizes various things I have tried with no effect if you're wondering. I've tried everything I can think of, but feel free to suggest something else.

I have observed this with both the DCAN and MIBSPI peripherals.

The following forms of waiting for the DMA channel to finish all give the same result:

  • Waiting for the bit in FTCFLAG to set
  • Waiting for the bit in BTCFLAG to set (I have minimized my test case to a single frame per block)
  • Waiting for the bit in FIFOASTAT to clear (My test is minimal enough it always ends up FIFO A)
  • Waiting for the bit in PEND to clear

The following forms of "short wait" all seem to make the problem go away when inserted between seeing the DMA channel is done and writing to the control packet:

  • 4 peripheral reads (but not 3)
  • 3 peripheral reads + dsb (but not 2)
  • 4 peripheral reads + a branch (but not 3)
  • 12 reads from normal memory (but not 11)

The following forms of writing to the channel descriptor all have the same result:

  • Writing the same value back to IDADDR
  • Writing a different value to IDADDR
  • Writing the same value to ITCOUNT
  • Writing a different value to ITCOUNT

Setting or clearing AIM doesn't make a difference.

I can reliably reproduce this either with the DMA buffer in writeback-mapped memory or with the caches disabled entirely. Note that to reproduce it with the caches disabled, I had to put all of the relevant code into RAM. I assume this is because executing from FLASH without the cache is too slow to hit the problem. I suspect the above timings for how long of a "short wait" is long enough are also different in this situation. I disabled both the i-cache and d-cache because it was easiest; I see no way the i-cache is relevant besides changing how long the code takes to run.

I eagerly await some clarification about what the DMA hardware is doing.

  • Hi Brian,

    I have reviewed the TRM descriptions of each of the flags you mentioned above. I would expect that there should be no issues with any of the methods you are using. Can you provide some simplified Halcogen based code that reproduces this issue so I can debug on my bench? I also want to discuss it further with one of our DMA and R5/Cache experts to see if there might be some interactions going on that we might not have expected or that we have missed in our TRM explanations.
  • Chuck,

    I can work on that but it might take a few days. Can you think of a simple DMA example I could start from?

    Brian

  • Brian,

    There is an example for MibSPI and DMA included with Halcogen but it uses DMA to transfer data into MibSPI for Tx instead of moving it out for Rx. Maybe this could be reconfigured so that the DMA was on thr Rx side instead of the send side?

    C:\ti\Hercules\HALCoGen\v04.07.00\examples\TMS570LC43x\example_mibspiDMA.c