Part Number: TM4C1294NCPDT
hello ,
I am working on deep sleep mode .I want to wake from deep sleep using hibernation wake pin.Is it possible ??
if possible ,tell me how it can be configured to wake from deep sleep ??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C1294NCPDT
hello ,
I am working on deep sleep mode .I want to wake from deep sleep using hibernation wake pin.Is it possible ??
if possible ,tell me how it can be configured to wake from deep sleep ??
This is the function created to enter into deep sleep mode but then also wake pin is not working Gpio pin is working but not every time ,sometime it works and sometime not.
void going_to_sleep()
{
sleep_init();
// Enable Auto Clock Gating Control.
SysCtlPeripheralClockGating(true);
// Set LDO to 0.90V in Deep-Sleep.
SysCtlLDODeepSleepSet(SYSCTL_LDO_0_90V);
// Set Flash & SRAM to Low Power in Deep-Sleep Mode.
SysCtlDeepSleepPowerSet(SYSCTL_FLASH_LOW_POWER | SYSCTL_SRAM_LOW_POWER);
#if(DEBUG)
{
DEBUG_PRINT_TIME();
DEBUG_PRINT((uint8_t *)"\t\t");
DEBUG_PRINT((uint8_t *)"Going to Sleep ");
DEBUG_PRINT((uint8_t *)"\r\n");
}
#endif
delay1(10);
led_on();
while(GPIOPinRead(GPIO_PORTE_BASE,GPIO_PIN_2)==GPIO_PIN_2); // Waits until camera is powered OFF
delay1(10);
SysCtlDeepSleep();
while(1)
{
#if(DEBUG)
{
DEBUG_PRINT_TIME();
DEBUG_PRINT((uint8_t *)"\t\t");
DEBUG_PRINT((uint8_t *)"Not entered in deep sleep mode ");
DEBUG_PRINT((uint8_t *)"\r\n");
}
#endif
}
}
********************************************
here i am initiated deep sleep mode
void sleep_init()
{
SysCtlDeepSleepClockConfigSet(1, (SYSCTL_DSLP_OSC_INT | SYSCTL_DSLP_PIOSC_PD | SYSCTL_DSLP_OSC_EXT32 ));
HibernateIntClear(HIBERNATE_INT_PIN_WAKE | HIBERNATE_INT_WR_COMPLETE | HIBERNATE_INT_RESET_WAKE);
SysCtlPeripheralDeepSleepEnable(SYSCTL_PERIPH_GPIOE);
SysCtlPeripheralDeepSleepEnable(SYSCTL_PERIPH_GPIOD);
SysCtlPeripheralDeepSleepEnable(SYSCTL_PERIPH_UART3);
SysCtlPeripheralDeepSleepEnable(SYSCTL_PERIPH_HIBERNATE);
HibernateEnableExpClk(freq);
HibernateClockConfig(HIBERNATE_OSC_LOWDRIVE);
HibernateRTCEnable();
SysCtlPeripheralDeepSleepDisable( SYSCTL_PERIPH_ADC0 | SYSCTL_PERIPH_ADC1 | SYSCTL_PERIPH_CAN0 | SYSCTL_PERIPH_CAN1 |
SYSCTL_PERIPH_CCM0 | SYSCTL_PERIPH_COMP0 | SYSCTL_PERIPH_EEPROM0 | SYSCTL_PERIPH_EMAC0 |
SYSCTL_PERIPH_EPHY0 | SYSCTL_PERIPH_EPI0 | SYSCTL_PERIPH_GPIOA | SYSCTL_PERIPH_GPIOB |
SYSCTL_PERIPH_GPIOC | SYSCTL_PERIPH_GPIOF | SYSCTL_PERIPH_GPIOG | SYSCTL_PERIPH_GPIOH |
SYSCTL_PERIPH_GPIOJ | SYSCTL_PERIPH_GPIOK | SYSCTL_PERIPH_GPIOL | SYSCTL_PERIPH_GPIOM |
SYSCTL_PERIPH_GPION | SYSCTL_PERIPH_GPIOR | SYSCTL_PERIPH_GPIOS | SYSCTL_PERIPH_WTIMER4 |
SYSCTL_PERIPH_GPIOT | SYSCTL_PERIPH_I2C0 | SYSCTL_PERIPH_I2C2 | SYSCTL_PERIPH_I2C3 |
SYSCTL_PERIPH_I2C4 | SYSCTL_PERIPH_I2C5 | SYSCTL_PERIPH_I2C6 | SYSCTL_PERIPH_I2C7 |
SYSCTL_PERIPH_I2C8 | SYSCTL_PERIPH_I2C9 | SYSCTL_PERIPH_LCD0 | SYSCTL_PERIPH_ONEWIRE0 |
SYSCTL_PERIPH_PWM0 | SYSCTL_PERIPH_PWM1 | SYSCTL_PERIPH_QEI0 | SYSCTL_PERIPH_QEI1 |
SYSCTL_PERIPH_SSI0 | SYSCTL_PERIPH_SSI1 | SYSCTL_PERIPH_SSI2 | SYSCTL_PERIPH_SSI3 |
SYSCTL_PERIPH_TIMER0 | SYSCTL_PERIPH_TIMER1 | SYSCTL_PERIPH_TIMER2 | SYSCTL_PERIPH_TIMER3 |
SYSCTL_PERIPH_TIMER4 | SYSCTL_PERIPH_TIMER5 | SYSCTL_PERIPH_TIMER6 | SYSCTL_PERIPH_TIMER7 |
SYSCTL_PERIPH_UART0 | SYSCTL_PERIPH_UART1 | SYSCTL_PERIPH_UART2 | SYSCTL_PERIPH_UART4 |
SYSCTL_PERIPH_UART5 | SYSCTL_PERIPH_UART6 | SYSCTL_PERIPH_UART7 | SYSCTL_PERIPH_UDMA |
SYSCTL_PERIPH_USB0 | SYSCTL_PERIPH_WDOG0 | SYSCTL_PERIPH_WDOG1 | SYSCTL_PERIPH_WTIMER0 |
SYSCTL_PERIPH_WTIMER1 | SYSCTL_PERIPH_WTIMER2 | SYSCTL_PERIPH_WTIMER3 | SYSCTL_PERIPH_WTIMER5 );
ptr_wake_up=ButtonIntHandler;
HibernateWakeSet( HIBERNATE_WAKE_PIN | HIBERNATE_WAKE_RTC | HIBERNATE_WAKE_RESET );
HibernateIntEnable(HIBERNATE_INT_PIN_WAKE | HIBERNATE_INT_RESET_WAKE);
HibernateIntRegister(ptr_wake_up );
GPIOPinTypeGPIOInput(GPIO_PORTE_BASE, GPIO_PIN_2);
GPIOIntClear(GPIO_PORTE_BASE,GPIO_INT_PIN_2);
// GPIODirModeSet(GPIO_PORTE_BASE, GPIO_PIN_2,GPIO_DIR_MODE_IN);
// GPIOPadConfigSet(GPIO_PORTE_BASE, GPIO_PIN_2,GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_WAKE_HIGH);
GPIOIntTypeSet(GPIO_PORTE_BASE, GPIO_PIN_2,GPIO_HIGH_LEVEL);
GPIOIntRegister(GPIO_PORTE_BASE,ptr_wake_up);
GPIOIntEnable(GPIO_PORTE_BASE,GPIO_INT_PIN_2);
IntMasterEnable();
}
************************************************************
This is my Interrupt handler :-
void ButtonIntHandler()
{
// Delay here on button push for simple debouncing.
delay1(1);
static uint32_t status1,Status;
Status = HibernateIntStatus(0);
if(1 == Status)
{
HibernateIntClear(Status);
}
status1=GPIOIntStatus(GPIO_PORTE_BASE,0);
if(1 == status1 )
{
GPIOIntClear(GPIO_PORTE_BASE,status1); // Clear the interrupts
}
led_on();
flag=1;
wakeup_flag=0;
wakeup_handle = 1;
#if(DEBUG)
{
DEBUG_PRINT_TIME();
DEBUG_PRINT((uint8_t *)"\t\t");
DEBUG_PRINT((uint8_t *)"Wake from deep sleep ");
DEBUG_PRINT((uint8_t *)"\r\n");
}
#endif
IntMasterEnable();
work_to_done();
}
cb1_mobile said:May we ask "from where did "3ca32tw" arise" - and what - if any - was its value in a "meaningless Subject Line?"
Indeed. It is hoped that the "LIKE Destroying" forum team would expend (some) effort in, "Advising posters that their Subject (i.e. their post's Headline) is a "Key Drawing Card" - and the "repetition of the MCU's id offers, "NO/ZERO INCENTIVE" to "Click" upon so "empty" a thread!
The addition of the cryptic "3ca xxx" - as you note - provides only further proof that "LIKE Destroyers" are WITHOUT a CLUE!