Part Number: EK-TM4C1294XL
Hello All,
I'am trying to use Hibernation Mode of TM4C129x Series MCU . My issue is that Iam getting a warning message argument of type "struct tm *" is incompatible with parameter of type "struct tm *" in my code as shown below and hence the hibernate mode not working
struct tm sTime;
uint32_t g_ui32MonthIdx, g_ui32DayIdx, g_ui32YearIdx;
uint32_t g_ui32HourIdx, g_ui32MinIdx,g_ui32SecIdx;
int main(Void)
{
//System clock already enabled
SysCtlPeripheralEnable(SYSCTL_PERIPH_HIBERNATE);
HibernateEnableExpClk(ui32SysClock);
HibernateClockConfig(HIBERNATE_OSC_LOWDRIVE);
HibernateRTCEnable();
// Configure the hibernate module counter to 24-hour calendar mode.
HibernateCounterMode(HIBERNATE_COUNTER_24HR);
HibernateCalendarSet(&sTime); //#169-D argument of type "struct tm *" is incompatible with parameter of type "struct tm *"
sTime.tm_mon = 11;
sTime.tm_mday = 17;
sTime.tm_year = 117;
sTime.tm_hour = 14;
sTime.tm_min = 34;
HibernateCalendarSet(&sTime);//#169-D argument of type "struct tm *" is incompatible with parameter of type "struct tm *"
while(1)
{
HibernateCalendarGet(&sTime);//#169-D argument of type "struct tm *" is incompatible with parameter of type "struct tm *"
g_ui32HourIdx = sTime.tm_hour ;
g_ui32MinIdx = sTime.tm_min ;
g_ui32MonthIdx = sTime.tm_mon;
g_ui32DayIdx = sTime.tm_mday;
g_ui32SecIdx = sTime.tm_sec;
sTime.tm_year = sTime.tm_year + 1900;
}
}
kindly help in resolving the issue.