Tool/software: Code Composer Studio
I am trying to communicate android and TM4C123GH6PM via ESP8266.
But I am getting Error #10234 although I have uartstdio.h and uartstdio.c in utils folder. And UARTStdioConfig, UARTprintf are well defined.
My Code is
//------------------- main.c --------------------------------- #include <stdint.h> #include <stdbool.h> #include <string.h> #include "inc/hw_gpio.h" #include "inc/hw_types.h" #include "inc/hw_memmap.h" #include "inc/hw_ints.h" #include "driverlib/fpu.h" #include "driverlib/debug.h" #include "driverlib/sysctl.h" #include "driverlib/pin_map.h" #include "driverlib/gpio.h" #include "driverlib/pwm.h" #include "driverlib/timer.h" #include "driverlib/adc.h" #include "utils/uartstdio.h" #include "utils/cmdline.h" #include "driverlib/uart.h" #include "driverlib/interrupt.h" #include "DelayTimer.h" static char COMMAND[128]; static char ReceivedData[512]; static char str[128]; bool process = true; bool ProcessRoutine(); char *Substring(char *src, char *dst, int start, int stop); int SearchIndexOf(char src[], char str[]); char* itoa(int i, char b[]); void ftoa(float f,char *buf); #define Period 320000 //(16000000/50) 50Hz void InitUART(void) { SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0); GPIOPinConfigure(GPIO_PA0_U0RX); GPIOPinConfigure(GPIO_PA1_U0TX); GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1); UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC); UARTStdioConfig(0, 115200, 16000000); } void InitESPUART(void) { SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB); SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1); GPIOPinConfigure(GPIO_PB0_U1RX); GPIOPinConfigure(GPIO_PB1_U1TX); GPIOPinTypeUART(GPIO_PORTB_BASE, GPIO_PIN_0 | GPIO_PIN_1); UARTClockSourceSet(UART1_BASE, UART_CLOCK_PIOSC); UARTConfigSetExpClk(UART1_BASE, 16000000, 115200, (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE)); UARTEnable(UART1_BASE); } void SendATCommand(char *cmd) { while(UARTBusy(UART1_BASE)); while(*cmd != '\0') { UARTCharPut(UART1_BASE, *cmd++); } UARTCharPut(UART1_BASE, '\r'); //CR UARTCharPut(UART1_BASE, '\n'); //LF } int recvString(char *target, char *data, int timeout, bool check) { int i=0; char a; unsigned long start = millis(); while (millis() - start < timeout) { while(UARTCharsAvail(UART1_BASE)) { a = UARTCharGet(UART1_BASE); if(a == '\0') continue; data[i]= a; i++; } if(check) { if (SearchIndexOf(data, target) != -1) { break; } } } return 0; } bool recvFind(char *target, int timeout,bool check) { recvString(target, ReceivedData, timeout, check); if (SearchIndexOf(ReceivedData, target) != -1) { return true; } return false; } bool recvFindAndFilter(char *target, char *begin, char* end, char *data, int timeout) { recvString(target, ReceivedData, timeout, true); if (SearchIndexOf(ReceivedData, target) != -1) { int index1 = SearchIndexOf(ReceivedData, begin); int index2 = SearchIndexOf(ReceivedData, end); if (index1 != -1 && index2 != -1) { index1 += strlen(begin); Substring(ReceivedData,data,index1, index2); return true; } } data = ""; return false; } bool ATesp(void) { memset(ReceivedData, 0, sizeof(ReceivedData)); SendATCommand("AT"); return recvFind("OK",5000, true); } bool RSTesp(void) { memset(ReceivedData, 0, sizeof(ReceivedData)); SendATCommand("AT+RST"); return recvFind("OK",5000, false); } bool CWMODEesp(void) { memset(ReceivedData, 0, sizeof(ReceivedData)); SendATCommand("AT+CWMODE=1"); return recvFind("OK",5000, true); } bool CWJAPesp(void) { memset(ReceivedData, 0, sizeof(ReceivedData)); SendATCommand("AT+CWJAP=\"Connectify-Gossu\",\"Goswami@h1\""); //Your Wifi: NetworkName, Password return recvFind("OK",10000, true); } bool CWQAPesp(void) { memset(ReceivedData, 0, sizeof(ReceivedData)); SendATCommand("AT+CWQAP"); return recvFind("OK",10000, true); } bool CIPMUXesp(void) { memset(ReceivedData, 0, sizeof(ReceivedData)); SendATCommand("AT+CIPMUX=0"); return recvFind("OK",5000, true); } bool ATGMResp(char *version) { memset(ReceivedData, 0, sizeof(ReceivedData)); SendATCommand("AT+GMR"); return recvFindAndFilter("OK", "\r\r\n", "\r\n\r\nOK", version,10000); } bool aCWMODEesp(char *list) { memset(ReceivedData, 0, sizeof(ReceivedData)); SendATCommand("AT+CWMODE=?"); return recvFindAndFilter("OK", "+CWMODE:(", ")\r\n\r\nOK", list,10000); } bool aCWLAPesp(char *list) { memset(ReceivedData, 0, sizeof(ReceivedData)); SendATCommand("AT+CWLAP"); return recvFindAndFilter("OK","\r\r\n", "\r\n\r\nOK", list,15000); } bool aCIFSResp(char *list) { memset(ReceivedData, 0, sizeof(ReceivedData)); SendATCommand("AT+CIFSR"); return recvFindAndFilter("OK","\r\r\n", "\r\n\r\nOK", list,15000); } bool CIPSTOesp(void) { memset(ReceivedData, 0, sizeof(ReceivedData)); SendATCommand("AT+CIPSTO=10000"); return recvFind("OK",2000, true); } bool CIPSTARTesp(void) { memset(ReceivedData, 0, sizeof(ReceivedData)); SendATCommand("AT+CIPSTART=4,\"TCP\",\"192.255.0.100\",9999"); //Server IP and Port: such as 192.255.0.100, 9999 return recvFind("OK",2000, true); } bool CIPCLOSEesp(void) { memset(ReceivedData, 0, sizeof(ReceivedData)); SendATCommand("AT+CIPCLOSE"); return recvFind("OK",5000, true); } bool CIPSENDesp(char *text) { int len = strlen(text)+2; itoa(len,str); char* AT_CMD_SEND = "AT+CIPSEND="; char CMD_TEXT[128]; strcpy(CMD_TEXT,AT_CMD_SEND); strcat(CMD_TEXT,str); memset(ReceivedData, 0, sizeof(ReceivedData)); SendATCommand(CMD_TEXT); delay(5); SendATCommand(text); return recvFind("SEND OK",2000, true); } void HardwareReset() { GPIOPinTypeGPIOOutput(GPIO_PORTD_BASE, GPIO_PIN_0); //Output GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_4, 0x00); //LOW ->Reset to ESP8266 SysCtlDelay(50); GPIOPinTypeGPIOOutput(GPIO_PORTD_BASE, GPIO_PIN_0); //Output ->// Open drain; reset -> GND delay(10); GPIOPinTypeGPIOInput(GPIO_PORTD_BASE, GPIO_PIN_0); //Input ->// Back to high-impedance pin state delay(3000); } void ProcessCommand(char *CommandText) { long Status; char *array[10]; int i=0; array[i] = strtok(CommandText,":"); while(array[i]!=NULL) { array[++i] = strtok(NULL,":"); } memset(COMMAND, 0, sizeof(COMMAND)); strncpy(COMMAND, array[1], (strlen(array[1])-1)); UARTprintf("CMD->%s\n",COMMAND); } QuitProcess() { process = false; } int main(void) { bool TaskStatus; SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ); SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF); GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE,GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3); GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, 0x00); GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0x00); GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3, 0x00); SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD); GPIOPinTypeGPIOOutput(GPIO_PORTD_BASE, GPIO_PIN_0); GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_0, 0x00); GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, 0x02); timerInit(); HardwareReset(); InitUART(); InitESPUART(); UARTprintf("Execute!\n"); delay(1000); TaskStatus = ATesp(); TaskStatus = RSTesp(); TaskStatus = CWMODEesp(); while(true) { UARTprintf("Trying to connect wi-fi\n"); TaskStatus = CWJAPesp(); if(TaskStatus) { UARTprintf("Connection is established!\n"); break; } } GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, 0x00); GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0x04); TaskStatus = CIPMUXesp(); while(true) { TaskStatus = ProcessRoutine(); if(TaskStatus) { CIPCLOSEesp(); GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3, 0x00); //Turn off Green Led GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0x04); //Turn on Blue Led } else { delay(10); CWQAPesp(); GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0x00); //Turn off Blue Led GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, 0x02); //Turn on Red Led } } } bool ProcessRoutine() { bool status; process = true; UARTprintf("Waiting Server...\n"); while(true) { status = CIPSTARTesp(); if(status) { UARTprintf("Communication is established!\n"); break; } delay(50); } GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0x00); GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3, 0x08); //TurnOn Green Led-> READY int i=0; char a; memset(ReceivedData, 0, sizeof(ReceivedData)); //Clear unsigned long start; while(process) { if(UARTCharsAvail(UART1_BASE)) { if (SearchIndexOf(ReceivedData, "+IPD,") != -1) { i=0; memset(ReceivedData, 0, sizeof(ReceivedData)); start = millis(); while (millis() - start < 5000) { while(UARTCharsAvail(UART1_BASE)) { a = UARTCharGet(UART1_BASE); if(a == '\0') continue; ReceivedData[i]= a; i++; } if (SearchIndexOf(ReceivedData, "\n") != -1) { break; } } ProcessCommand(ReceivedData); i=0; memset(ReceivedData, 0, sizeof(ReceivedData)); } else { a = UARTCharGet(UART1_BASE); if(a == '\0') continue; ReceivedData[i]= a; i++; } } } return true; } char *Substring(char *src, char *dst, int start, int stop) { int len = stop - start; strncpy(dst, src + start, len); return dst; } int SearchIndexOf(char src[], char str[]) { int i, j, firstOcc; i = 0, j = 0; while (src[i] != '\0') { while (src[i] != str[0] && src[i] != '\0') i++; if (src[i] == '\0') return (-1); firstOcc = i; while (src[i] == str[j] && src[i] != '\0' && str[j] != '\0') { i++; j++; } if (str[j] == '\0') return (firstOcc); if (src[i] == '\0') return (-1); i = firstOcc + 1; j = 0; } return (-1); } char* itoa(int i, char b[]) { char const digit[] = "0123456789"; char* p = b; if(i<0){ *p++ = '-'; i *= -1; } int shifter = i; do{ ++p; shifter = shifter/10; }while(shifter); *p = '\0'; do{ *--p = digit[i%10]; i = i/10; }while(i); return b; } void ftoa(float f,char *buf) { int pos=0,ix,dp,num; if (f<0) { buf[pos++]='-'; f = -f; } dp=0; while (f>=10.0) { f=f/10.0; dp++; } for (ix=1;ix<8;ix++) { num = f; f=f-num; if (num>9) buf[pos++]='#'; else buf[pos++]='0'+num; if (dp==0) buf[pos++]='.'; f=f*10.0; dp--; } } //-------------------- main.h --------------------------- #ifndef MAIN_H_ #define MAIN_H_ extern QuitProcess(void); #endif /* MAIN_H_ */ //-------------------------- DelayTimer.c ------------------------------------------ #include <stdint.h> #include <stdbool.h> #include <math.h> #include "inc/hw_ints.h" #include "inc/hw_timer.h" #include "inc/hw_types.h" #include "inc/hw_memmap.h" #include "driverlib/rom.h" #include "driverlib/sysctl.h" #include "driverlib/timer.h" #include "driverlib/interrupt.h" #include "inc/hw_nvic.h" static unsigned long milliseconds = 0; void timerInit(void) { SysTickPeriodSet(0x00FFFFFF); SysTickEnable(); SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER5); TimerConfigure(TIMER5_BASE, TIMER_CFG_PERIODIC_UP); TimerLoadSet(TIMER5_BASE, TIMER_A, SysCtlClockGet()/1000); IntEnable(INT_TIMER5A); TimerIntEnable(TIMER5_BASE, TIMER_TIMA_TIMEOUT); TimerEnable(TIMER5_BASE, TIMER_A); IntMasterEnable(); } unsigned long micros(void) { return (milliseconds * 1000) + (HWREG(TIMER5_BASE + TIMER_O_TAV) / 80); } unsigned long millis(void) { return milliseconds; } void delayMicroseconds(unsigned int us) { volatile unsigned long elapsedTime; unsigned long startTime = HWREG(NVIC_ST_CURRENT); do{ elapsedTime = startTime-(HWREG(NVIC_ST_CURRENT) & 0x00FFFFFF); } while(elapsedTime <= us*80); } void delay(uint32_t milliseconds) { unsigned long i; for(i=0; i<milliseconds; i++){ delayMicroseconds(1000); } } void Timer5IntHandler(void) { TimerIntClear(TIMER5_BASE, TIMER_TIMA_TIMEOUT); milliseconds++; } //---------------------------- DelayTimer.h -------------------------------------------- #ifndef DELAYTIMER_H_ #define DELAYTIMER_H_ extern void timerInit(void); extern unsigned long micros(void); extern unsigned long millis(void); extern void delayMicroseconds(unsigned int us); extern void delay(uint32_t milliseconds); #endif /* DELAYTIMER_H_ */
Here I am attaching the screenshot of console window.
Any help will be highly appreciated.