Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
Hi,
i am using the following version for my application development.
CCS - 6.2
TI RTOS - tirtos_tivac_2_16_01_14
ndk - ndk_2_25_00_09
BIOS - bios_6_45_02_31
i want to create the task dynamically from another task using Task_create() API. but its returning NULL and task is not been created. find the below code used to create the task.
Task_Handle userPgmHandle;
Task_Params userPgmParams;
Task_Params_init(&userPgmParams);
userPgmParams.stackSize = 2048;
userPgmParams.priority = 5;
userPgmHandle =
Task_create((Task_FuncPtr)UserFunc, &userPgmParams, &eb);
if (userPgmHandle == NULL) {
System_printf("User Program Start failed\n");
}
but the same code is creating the task when its added in tcpHandlerHook function.
i also added the follwoing code to CFG file.
/* Allow for run-time creates/memory allocation */
var Defaults = xdc.useModule('xdc.runtime.Defaults');
var Types = xdc.useModule('xdc.runtime.Types');
Defaults.common$.memoryPolicy = Types.CREATE_POLICY;
BIOS.runtimeCreatesEnabled = true;
if i added the above code to cfg file then i am getting the following error while running..
ti.sysbios.knl.Semaphore: delete policy error
xdc.runtime.Error.raise: terminating execution
what is missed here?
Regards
Bala