Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN,
Hello
Could you please help my customer with the following problem
TMS570LS3137 SPI RX and TX Flags. spi.c code generated by HALCoGen version 04.05.01, 28.Aug.2015. CCS version 6.1.0.00104 on a standalone laptop.
When calling the spiTransmitData function, the code successfully checks for error flags
if((spi->FLG & 0x000000FFU) !=0U)
{
break;
},
gets the new data to send, then, logically, it should check the TX flag to determine whether the outputting “shift register” is clear for the new data:
/*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
while((spi->FLG & 0x00000100U) != 0x00000100U)
{
} /* Wait */
According to the Technical Reference Manual, spnu499b, November 2012–Revised August 2013, bit 0x00000100 is the RXINTFLG, which in my hardware is FALSE as I would expect it to be. So I tried hacking this line to become the TX flag – it ran through for the first word but then crashed.
If I use code written for me (from which I cribbed this section), the RX flag is FALSE until the chunk
spi->DAT1 = ((uint32)DataFormat << 24U) |
((uint32)ChipSelect << 16U) |
(WDelay) |
(Chip_Select_Hold) |
(uint32)Tx_Data;
Is executed, whereupon it’s set TRUE… Don’t understand… The only difference I know about is the original uses Chip_Select_Hold true, whereas mine needs to be false.
I notice that the BUFINITACTIVE flag remains set throughout the working code, but not in mine. I haven’t chosen to use the Multi-buffering feature: only the base SPI drivers have been enabled in HALCoGen (for both projects). The TXINTFLG is never obviously used.
I am calling the spiInit function as required.
Any suggestions, please.
Regards
Bob Bacon