Part Number: RM57L843
Hi
There are two things with reference to GPIO and EMIF.
1)- The datasheet of RM57L843 says the number of eight-bit GIO Ports are only two with 16 interrupts and having 161 GPIO in total. While the doc spnu562 considers the possibility of 08 ports of eight bit with 32 interrupts possible. It means that all the 145 pins are only available on the pin basis when not used in their original functionality or they can be used on the port basis.
2)- The datasheet says that it provides three CS of Async interface providing 16MB on each of the three CS on EMIF, while the document spnu562 does specify the provision of external memory with GPIO without mentioning any size. When I asked for the support, I have been told that 64MB is possible (as the address range also confirm this). I'm confused with the page 90 of datasheet where it claims to have 64MB frame size and 16MB of actual size. What is the difference between the frame and actual size? and is it possible to use the 64MB 16-bit device?
Regards;
Regards;