This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LS0432: Linker command file configuration

Part Number: TMS570LS0432

Tool/software: Code Composer Studio

Hi , I have loaded UART bootloader into TMS570ls0432 lower flash memory . I have attached memory configuration also . 

But I have confusion about linker command file for other new images to be loaded . 

Here is linker.cmd for bootloader 

MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000200
BOOT_LOAD (RX) : origin=0x00000200 length=0x00001000
FLASH_API (RX) : origin=0x00001200 length=0x00001000
FLASH0 (RX) : origin=0x00002200 length=0x00050000
SRAM (RW) : origin=0x08002000 length=0x0005c000
STACK (RW) : origin=0x08000000 length=0x00001FF0
}

And this here is new application  project linker,cmd file 

MEMORY
{
VECTORS (X) : origin=0x00002000 length=0x00000200
FLASH0 (RX) : origin=0x00002200 length=0x0005FFE0
STACKS (RW) : origin=0x08000000 length=0x00001500
RAM (RW) : origin=0x08001500 length=0x00006B00

}

But it is not working . 

I have not clear idea of how to configure new linker command file .

Does i need to add again VECTORS (X) in new project ? (Reset vector must be same for both )

when I am loading new project with above configuration using ccs to test it is erasing my bootloader .

Thank you .