Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: UNIFLASH
Hello,
I am trying to program the MAC address of a TM4C1294 Tiva Microcontroller using the LM flash programmer tool. This works fine when I do this on an MCU that is in the launchpad (Set configration to TM4C1294 Launchpad.) However, I would like to do the same using the XDS110 probe. Is this possible? Can the LM flash programmer tool be used to program / clear the MAC address registers of a Tiva-C device via the XDS 110?
I am able to program my Tiva-C MCU using the XDS110 from within code composer studio fine, but it is unclear if it is possible to do so using XDS 110.
Thank you,
svl123