Part Number: RM57L843
Hi
With reference to SPNU562 a note on page 295 (IOMM) is written as:
""The input signals are broadcast to all modules hooked up to a terminal. The application must ensure that modules that are not being used in the application do not react to a change on
their input functions. e.g. a GIO signal toggle can trigger an interrupt request, when the application actually is using the function multiplexed with this GIO signal.""
With reference to this note I'm unable to understand the can i use two modules simultaneously. As pin signal is broadcasted to all modules, without a multiplexer. As shown in Fig 6-3.
So, I'm confused by this statement " The application must ensure that modules that are not being used in the application do not react to a change in their input functions".
What are the precautions in hardware if any?
Regards;