Part Number: RM48L730
Tool/software: TI C/C++ Compiler
Hi,
I am using F021 flash api in a RM48L730 projects compiled with arm-gcc-eabi.
when I disassembly my project, some instructions in the library function are undefined.
example : Fapi_issueAsyncCommandWithAddress function
Disassembly of section .text:Fapi_issueAsyncCommandWithAddress:
08001f08 <Fapi_issueAsyncCommandWithAddress>:
8001f08: b538 push {r3, r4, r5, lr}
8001f0a: 4605 mov r5, r0
8001f0c: 460c mov r4, r1
8001f0e: 2d06 cmp r5, #6
8001f10: d005 beq.n 8001f1e <Fapi_issueAsyncCommandWithAddress+0x16>
8001f12: 2d08 cmp r5, #8
8001f14: d003 beq.n 8001f1e <Fapi_issueAsyncCommandWithAddress+0x16>
8001f16: 2d0e cmp r5, #14
8001f18: bf18 it ne
8001f1a: 2005 movne r0, #5
8001f1c: d108 bne.n 8001f30 <Fapi_issueAsyncCommandWithAddress+0x28>
8001f1e: 2010 movs r0, #16
8001f20: f7ff faee bl 8001500 <_Fapi_issueFsmCommand>
8001f24: 4803 ldr r0, [pc, #12] ; (8001f34 <Fapi_issueAsyncCommandWithAddress+0x2c>)
8001f26: 6004 str r4, [r0, #0]
8001f28: 4628 mov r0, r5
8001f2a: f7ff fae9 bl 8001500 <_Fapi_issueFsmCommand>
8001f2e: 2000 movs r0, #0
8001f30: bd38 pop {r3, r4, r5, pc}
8001f32: 46c0 nop ; (mov r8, r8)
8001f34: fff87110 ; <UNDEFINED> instruction: 0xfff87110 ; it generate a prefetched exception
8001f38: 00003241 andeq r3, r0, r1, asr #4
with code studio composer (armdis tools), it gives the following assembly :
8001f08: Fapi_issueAsyncCommandWithAddress:
8001f08: .thumb
8001f08: 38B5 PUSH {R3, R4, R5, LR}
8001f0a: 0546 MOV R5, R0
8001f0c: 0C46 MOV R4, R1
8001f0e: 062D CMP R5, #6
8001f10: 05D0 BEQ 0x08001F1E
8001f12: 082D CMP R5, #8
8001f14: 03D0 BEQ 0x08001F1E
8001f16: 0E2D CMP R5, #14
8001f18: 18BF IT NE
8001f1a: 0520 MOVNE R0, #5
8001f1c: 08D1 BNE 0x08001F30
8001f1e: $C$L1:
8001f1e: 1020 MOVS R0, #16
8001f20: FFF7EEFA BL 0x08001500
8001f24: 0348 LDR R0, $C$CON1 [0x8001f34]
8001f26: 0460 STR R4, [R0]
8001f28: 2846 MOV R0, R5
8001f2a: FFF7E9FA BL 0x08001500
8001f2e: 0020 MOVS R0, #0
8001f30: $C$L2:
8001f30: 38BD POP {R3, R4, R5, PC}
8001f32: C046 MOV R8, R8
8001f34: $d: ; equivalent line of the undefined instruction above
8001f34: $C$CON1:
8001f34: 1071 .half 0x7110
8001f36: F8FF .half 0xFFF8
8001f38: $d:
8001f38: 4132 .half 0x3241
8001f3a: 0000 .half 0x0000
8001f3c: 0054 .half 0x5400
8001f3e: 4900 .half 0x0049
how to resolve this issue ?