This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TM4C123GH6PM: Trouble configuring ADC and uDMA for continuous transfer; ADC int won't trigger

Part Number: TM4C123GH6PM


I'm trying to configure the uDMA to transfer 1024 values (16 bits each). I'm having some trouble as the code won't get the ADC INT to trigger. I have a breakpoint in the interrupt and it never reaches it.

The ADC is being triggered by a Timer and I would like the uDMA to capture a value everytime it gets triggered. Is there something wrong in the initialization code? Thank you

Also, I'm trying to use ADC0 and Sequencer 3. So it will be capture 1 value. In addition, my sampling rate is approx 50 kHz.

Thank you, I really appreciate it

Tool/software: TI-RTOS


void ConfigureADCandDMA(void) { // Enable uDMA and ADC peripheral SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0); SysCtlPeripheralReset(SYSCTL_PERIPH_ADC0); ADCClockConfigSet(ADC0_BASE, ADC_CLOCK_SRC_PLL | ADC_CLOCK_RATE_FULL, 30); // uDMA initialize ADCSequenceConfigure(ADC0_BASE, 3, ADC_TRIGGER_TIMER, 0); ADCSequenceStepConfigure(ADC0_BASE, 3, 0, ADC_CTL_CH8 | ADC_CTL_IE | ADC_CTL_END); ADCSequenceDMAEnable(ADC0_BASE, 3); // ##################################################### SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA); SysCtlPeripheralReset(SYSCTL_PERIPH_UDMA); uDMAEnable(); uDMAControlBaseSet(sControlTable); uDMAChannelAttributeDisable(UDMA_CHANNEL_ADC0, UDMA_ATTR_ALL); uDMAChannelAttributeEnable(UDMA_CHANNEL_ADC0, UDMA_ATTR_USEBURST /*only allow burst transfers*/); uDMAChannelControlSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT, UDMA_SIZE_16 | UDMA_SRC_INC_NONE | UDMA_DST_INC_16 | UDMA_ARB_1024); uDMAChannelTransferSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT, UDMA_MODE_BASIC, (void *)(ADC0_BASE + ADC_O_SSFIFO3), g_ulADCValues, 1023); uDMAChannelEnable(UDMA_CHANNEL_ADC0); IntEnable(INT_UDMAERR); IntEnable(INT_UDMA); IntEnable(INT_ADC0SS3); ADCIntEnableEx(ADC0_BASE, ADC_INT_DMA_SS3); ADCSequenceEnable(ADC0_BASE, 3); // ADCIntEnable(ADC0_BASE, 3); ADCIntClear(ADC0_BASE, 3); }