Part Number: LAUNCHXL2-RM57L
Other Parts Discussed in Thread: HALCOGEN, C2000WARE
I am using the LAUNCHXL2-RM57L connects to F28377D via SPI and each MCU has to be Slave or Master bi-directional setting.
Given the F28377D clock rate of SPI is 50MHz in High-speed mode and the SPI clock rate is set under 1/4th of its maximum rate (i.e. 82.5MHz) in general,
That is, for compromising reasons, the SPI clock rate has to be under 50MHz is right?
If right, how can I use the GUI tool "HalCoGen" for doing this setting?
Thanks.