Part Number: RM46L852
Team,
Could you please answer my customer question,
I would need some help with the power sequencing of the RM46L852PGE controller.
The statement in the datasheet says that the device may be powered up in any order on the supplies. I have a colleague writing software, who managed to destroy some controllers. I am not sure, if this is not a problem caused by him during testing. But I am doing a review at the moment to see, if there is any critical point.
In the past, we had some contact about the power management IC TPS65381. The result from that was that a colleague from TI recommended to use an external buck regulator to supply the core voltage. I start this buck together with the ignition signal at the TPS. The result is that the TPS starts quite some milliseconds later.
(Ch1: 3V3 output of the TPS, Ch2: 1.2Volts core, Ch3: 5Volts for the ADC supply, Ch4: other ICs are connected to this 3V3, enabled by rising 3V3 from the TPS)
If one really may power up in any order, this should not be a problem. But I have to do a redesign for some other reasons. So there would be room for improvements.
Is there a risk with this sequence that is not obvious in the datasheet?
Another question is: If this colleague makes a mistake to switch a pin to output, which is connected to another output. Is this a problem that results in failed device? (For example a pin switched to output high that is pulled down to GND) It should not happen, but as you know… everything is possible J
I never managed to damage a controller by myself. So if you asked me about that, I would say that there is not a problem. So I would appreciate some advice with that. Thank you!
Thank you,
- Needhu