This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Partnumber of J9, J10, J11 on TMDXRM46HDK

Other Parts Discussed in Thread: TMDXRM46HDK

Hi eveyOne

Does AnyOne know the partnumber of J9,J10,J11 of TMDXRM46HDK board? Or any advice for the opposite side part? 

I think the pins distance on J9,J10,J11  is 2mm, but the distance of J10 pin65 to J11 pin2 is not multiple of 2.0mm. 

What should i do, it is not fixed universal board.

Thank you very much!

  • Hello Quan,

    I am forwarding your questions to the board designer so they can provide further information. However, board design files are available on the product page for this HDK at this link . There is also a user guide with some additional board information contained within it.

    nguyen quan said:

    I think the pins distance on J9,J10,J11  is 2mm, but the distance of J10 pin65 to J11 pin2 is not multiple of 2.0mm. 

    What should i do, it is not fixed universal board.

    I am not certain what you are referring to in this set of questions/comments. It is a custom design by TI for Hercules development. Each of the connectors are included to provide access to specified functionality. For certain, you can design a compatible board as a "daughter" card using these connectors for system level development (although production use of the HDKs is not permitted by license). It is not designed to comply with any standard or be universal outside of the Hercules family of devices.

  • Thanks so much for your answer.