Part Number: TMDX570LC43HDK
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
Hi.
I'm using a TMDX570LC43HDK and try to communicate with another board via SCI3 port. So, in HCG I enable the "SCI3 driver", in "VIM Channel 64" the Interrupt and in "SCI3 configuration" I enable RX interrupt. I also enable in PINMUX SCI3 to use NHET1[6] as RX pin and NHET1[13] as TX pin. But, I just got nothing. I certainly miss something in my configurations but I just don't know what. I also try to self-test SCI3 and got nothing too.
I join here my self-test code.
Really need some help here.
Regards,
OJ