Part Number: TM4C129XNCZAD
the code is just a modification of dma_demo from TM4c129X lib, UART0 works fine.. not the UART5 though.. anything I am missing in configuration part?
I checked TX output pin and there is no signal out, always high (3.3V)
ISR for receiving
void UART5IntHandler(void)
{
uint32_t ui32Status1;
uint32_t ui32Mode1;
//
// Read the interrupt status of the UART.
//
ui32Status1 = ROM_UARTIntStatus(UART5_BASE, 1);
//UARTIntDisable(UART0_BASE);
if (ui32Status1 == 0x00020000)
{
// do something here..........
ROM_UARTDMADisable(UART5_BASE, UART_DMA_TX);
// Need this step to be able to exit the interrupt.
ROM_UARTIntClear(UART5_BASE, ui32Status1);
return;
}
//HWREG(UART0_BASE + UART_O_ICR) = 0x00020000;
//ui32Status = ROM_UARTIntStatus(UART0_BASE, 1);
//
// Clear any pending status, even though there should be none since no UART
// interrupts were enabled. If UART error interrupts were enabled, then
// those interrupts could occur here and should be handled. Since uDMA is
// used for both the RX and TX, then neither of those interrupts should be
// enabled.
//
ROM_UARTIntClear(UART5_BASE, ui32Status1);
ui32Status1 = ROM_UARTIntStatus(UART5_BASE, 1);
//
// Check the DMA control table to see if the ping-pong "A" transfer is
// complete. The "A" transfer uses receive buffer "A", and the primary
// control structure.
//
ui32Mode1 = ROM_uDMAChannelModeGet(UDMA_CH6_UART5RX | UDMA_PRI_SELECT);
//
// If the primary control structure indicates stop, that means the "A"
// receive buffer is done. The uDMA controller should still be receiving
// data into the "B" buffer.
//
if (ui32Mode1 == UDMA_MODE_STOP)
{
//
// Increment a counter to indicate data was received into buffer A. In
// a real application this would be used to signal the main thread that
// data was received so the main thread can process the data.
// -------------------------> Set the data recieved flag in Buffer A--->>???
//g_ui32RxBufACount++;
//
// Set up the next transfer for the "A" buffer, using the primary
// control structure. When the ongoing receive into the "B" buffer is
// done, the uDMA controller will switch back to this one. This
// example re-uses buffer A, but a more sophisticated application could
// use a rotating set of buffers to increase the amount of time that
// the main thread has to process the data in the buffer before it is
// reused.
//
ROM_uDMAChannelTransferSet(UDMA_CH6_UART5RX | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
(void *) (UART5_BASE + UART_O_DR),
g_ui8pMeterRxBufA,
sizeof(g_ui8pMeterRxBufA));
}
//
// Check the DMA control table to see if the ping-pong "B" transfer is
// complete. The "B" transfer uses receive buffer "B", and the alternate
// control structure.
//
ui32Mode1 = ROM_uDMAChannelModeGet(UDMA_CH6_UART5RX | UDMA_ALT_SELECT);
//
// If the alternate control structure indicates stop, that means the "B"
// receive buffer is done. The uDMA controller should still be receiving
// data into the "A" buffer.
//
if (ui32Mode1 == UDMA_MODE_STOP)
{
//
// Increment a counter to indicate data was received into buffer A. In
// a real application this would be used to signal the main thread that
// data was received so the main thread can process the data.
//
//g_ui32RxBufBCount++;
//// -------------------------> Set the data recieved flag--->>???
// Set up the next transfer for the "B" buffer, using the alternate
// control structure. When the ongoing receive into the "A" buffer is
// done, the uDMA controller will switch back to this one. This
// example re-uses buffer B, but a more sophisticated application could
// use a rotating set of buffers to increase the amount of time that
// the main thread has to process the data in the buffer before it is
// reused.
//
ROM_uDMAChannelTransferSet(UDMA_CH6_UART5RX | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(void *) (UART5_BASE + UART_O_DR),
g_ui8pMeterRxBufB,
sizeof(g_ui8pMeterRxBufB));
}
//
// If the UART0 DMA TX channel is disabled, that means the TX DMA transfer
// is done.
//
// The uDMA TX channel must be re-enabled.
//
}
// function to configure the UART 5 for write and read using DMA
void InitUART5Transfer(void)
{
// Configure Device pins for Meter UART
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
ROM_GPIOPinConfigure(GPIO_PC6_U5RX);
ROM_GPIOPinConfigure(GPIO_PC7_U5TX);
ROM_GPIOPinTypeUART(GPIO_PORTC_BASE, GPIO_PIN_6 | GPIO_PIN_7);
// Enable the UDMA UART & configure it to operate even if the CPU is in sleep
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UDMA);
ROM_IntEnable(INT_UDMAERR);
//
// Enable the uDMA controller.
//
ROM_uDMAEnable();
ROM_uDMAControlBaseSet(pui8ControlTable);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART5);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UART5);
// Configure the UART communication parameters.
//
ROM_UARTConfigSetExpClk(UART5_BASE, ui32SysClock, 9600,
UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE);
//Enable the uDMA controller error interrupt. This interrupt will occur
// if there is a bus error during a transfer.
//
//
// Point at the control table to use for channel control structures.
//
//
// Set both the TX and RX trigger thresholds to 4. This will be used by
// the uDMA controller to signal when more data should be transferred. The
// uDMA TX and RX channels will be configured so that it can transfer 4
// bytes in a burst when the UART is ready to transfer more data.
//
ROM_UARTFIFOLevelSet(UART5_BASE, UART_FIFO_TX1_8, UART_FIFO_RX1_8);
//
// Enable the UART for operation, and enable the uDMA interface for both TX
// and RX channels.
//
ROM_UARTEnable(UART5_BASE);
//ROM_UARTDMAEnable(UART0_BASE, UART_DMA_RX );
ROM_UARTDMAEnable(UART5_BASE, UART_DMA_RX | UART_DMA_TX);
//
// This register write will set the UART to operate in write mode.
//
//HWREG(UART0_BASE + UART_O_CTL) |= UART_CTL_TXE;
//
// Put the attributes in a known state for the uDMA UART0RX channel. These
// should already be disabled by default.
//
ROM_uDMAChannelAttributeDisable(UDMA_CH6_UART5RX,
UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK);
//
// Configure the control parameters for the primary control structure for
// the UART RX channel. The primary contol structure is used for the "A"
// part of the ping-pong receive. The transfer data size is 8 bits, the
// source address does not increment since it will be reading from a
// register. The destination address increment is byte 8-bit bytes. The
// arbitration size is set to 4 to match the RX FIFO trigger threshold.
// The uDMA controller will use a 4 byte burst transfer if possible. This
// will be somewhat more effecient that single byte transfers.
//
ROM_uDMAChannelControlSet(UDMA_CH6_UART5RX | UDMA_PRI_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
UDMA_ARB_1);
//
// Configure the control parameters for the alternate control structure for
// the UART RX channel. The alternate contol structure is used for the "B"
// part of the ping-pong receive. The configuration is identical to the
// primary/A control structure.
//
ROM_uDMAChannelControlSet(UDMA_CH6_UART5RX | UDMA_ALT_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
UDMA_ARB_1);
//
// Set up the transfer parameters for the UART RX primary control
// structure. The mode is set to ping-pong, the transfer source is the
// UART data register, and the destination is the receive "A" buffer. The
// transfer size is set to match the size of the buffer.
//
ROM_uDMAChannelTransferSet(UDMA_CH6_UART5RX | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
(void *) (UART5_BASE + UART_O_DR),
g_ui8pMeterRxBufA, sizeof(g_ui8pMeterRxBufA));
//
// Set up the transfer parameters for the UART RX alternate control
// structure. The mode is set to ping-pong, the transfer source is the
// UART data register, and the destination is the receive "B" buffer. The
// transfer size is set to match the size of the buffer.
//
ROM_uDMAChannelTransferSet(UDMA_CH6_UART5RX | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(void *) (UART5_BASE + UART_O_DR),
g_ui8pMeterRxBufB, sizeof(g_ui8pMeterRxBufB));
//
// Put the attributes in a known state for the uDMA UART0TX channel. These
// should already be disabled by default.
//
ROM_uDMAChannelAttributeDisable(UDMA_CH7_UART5TX,
UDMA_ATTR_ALTSELECT |
UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK);
//
// Set the USEBURST attribute for the uDMA UART TX channel. This will
// force the controller to always use a burst when transferring data from
// the TX buffer to the UART. This is somewhat more effecient bus usage
// than the default which allows single or burst transfers.
//
ROM_uDMAChannelAttributeEnable(UDMA_CH7_UART5TX, UDMA_ATTR_USEBURST);
//
// Configure the control parameters for the UART TX. The uDMA UART TX
// channel is used to transfer a block of data from a buffer to the UART.
// The data size is 8 bits. The source address increment is 8-bit bytes
// since the data is coming from a buffer. The destination increment is
// none since the data is to be written to the UART data register. The
// arbitration size is set to 4, which matches the UART TX FIFO trigger
// threshold.
//
ROM_uDMAChannelControlSet(UDMA_CH7_UART5TX | UDMA_PRI_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_8 |
UDMA_DST_INC_NONE |
UDMA_ARB_1);
//
// Set up the transfer parameters for the uDMA UART TX channel. This will
// configure the transfer source and destination and the transfer size.
// Basic mode is used because the peripheral is making the uDMA transfer
// request. The source is the TX buffer and the destination is the UART
// data register.
ROM_uDMAChannelTransferSet(UDMA_CH7_UART5TX | UDMA_PRI_SELECT,
UDMA_MODE_BASIC,
g_ui8pMeterTxBuf,
(void *) (UART5_BASE + UART_O_DR),
sizeof(g_ui8pMeterTxBuf));
// Now both the uDMA UART TX and RX channels are primed to start a
// transfer. As soon as the channels are enabled, the peripheral will
// issue a transfer request and the data transfers will begin.
//
ROM_uDMAChannelEnable(UDMA_CH6_UART5RX);
ROM_uDMAChannelEnable(UDMA_CH7_UART5TX);
//
// Enable the UART DMA TX/RX interrupts.
//
//ROM_UARTIntEnable(UART0_BASE, UART_INT_DMATX | UART_INT_DMARX);
ROM_UARTIntEnable(UART5_BASE, UART_INT_DMARX);
//
// Enable the UART peripheral interrupts.
//
ROM_IntEnable(INT_UART5);
}