Part Number: TM4C123GH6ZRB
Team,
my customer is using Tiva in a new project that is going into production now. In order to enable their customers to do firmware updates via USB, they need to provide a driver to them. They don't want to have each customer install TivaWare, so they want to extract the driver from our suite and provide it to their customers.
This includes
- ...\TivaWare_C_Series-2.1.4.178\windows_drivers\amd64
- ...\TivaWare_C_Series-2.1.4.178\windows_drivers\i386
- ...\TivaWare_C_Series-2.1.4.178\windows_drivers\boot_usb.cat
- ...\TivaWare_C_Series-2.1.4.178\windows_drivers\boot_usb.inf
Is TI ok with this?'
Are there alternative packages including only "...\TivaWare_C_Series-2.1.4.178\windows_drivers" so they can link their customers to TI for driver download?
Is there an alternative solution?
Thanks for your support!