Part Number: TM4C129EKCPDT
We're using the TM4C129EKCPDTI3 for a project requiring the use of both of the CAN buses and the USB as a host (OTG not required) simultaneously. I noticed that pins 95 (CAN1Rx/USB0ID) and 96 (CAN1Tx/USB0VBUS) are common to both the USB and one of the CANs. However, after reading this maxim document, I get the impression that the USB ID and USB VBUS lines are only required for USB OTG.
Is it possible to use the USB as a host without pins 95 and 96?
Thank you,
Alex