Part Number: EK-TM4C123GXL
I am having problem receiving characters on the UART port 2 Rx pin. I have connected (hardware) pins PB1 (Tx ox UART1) to PD6 (Rx of UART2). I am transmitting data from the UART1 port succesfully, but unable to receive anything on the UART port 2 Rx pin. I am posting the code too. Even a small help would be appreciated in this direction.
#include <stdbool.h>
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
#include "driverlib/interrupt.h"
#include "inc/hw_ints.h"
#include "driverlib/rom_map.h"
#include "utils/uartstdio.h"
//*****************************************************************************
//*****************************************************************************
//
// This function sets up UART1 to be used for communication between launchpad
// and GPS Module.
//
//*****************************************************************************
void
ConfigureUART1(void)
{
//
// Enable GPIO port B which is used for UART1 pins.
// TODO: change this to whichever GPIO port you are using.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
//
// Configure the pin muxing for UART1 functions on port B0 and B1.
// This step is not necessary if your part does not support pin muxing.
// TODO: change this to select the port/pin you are using.
//
GPIOPinConfigure(GPIO_PB0_U1RX);
GPIOPinConfigure(GPIO_PB1_U1TX);
//
// Enable UART1 so that we can configure the clock.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);
//
// Use the internal 16MHz oscillator as the UART clock source.
// Check with sir
//
UARTClockSourceSet(UART1_BASE, UART_CLOCK_PIOSC);
//
// Select the alternate (UART) function for these pins.
// TODO: change this to select the port/pin you are using.
//
GPIOPinTypeUART(GPIO_PORTB_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Initialize the UART1.
//
//UARTStdioConfig(1, 9600, 16000000);
UARTClockSourceSet(UART1_BASE, UART_CLOCK_PIOSC);
UARTConfigSetExpClk(UART1_BASE, UART_CLOCK_PIOSC ,9600,UART_CONFIG_PAR_ZERO);
UARTFIFOEnable(UART1_BASE);
}
//*****************************************************************************
//
// This function sets up UART2 to be used for communication between UART1 and UART2.
//
//*****************************************************************************
void
ConfigureUART2(void)
{
//
// Enable GPIO port D which is used for UART2 pins.
// TODO: change this to whichever GPIO port you are using.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
//
// Configure the pin muxing for UART2 functions on port D6 and D7.
// This step is not necessary if your part does not support pin muxing.
// TODO: change this to select the port/pin you are using.
//
GPIOPinConfigure(GPIO_PD6_U2RX);
GPIOPinConfigure(GPIO_PD7_U2TX);
//
// Enable UART1 so that we can configure the clock.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART2);
//
// Use the internal 16MHz oscillator as the UART clock source.
// Check with sir
//
UARTClockSourceSet(UART2_BASE, UART_CLOCK_PIOSC);
//
// Select the alternate (UART) function for these pins.
// TODO: change this to select the port/pin you are using.
//
GPIOPinTypeUART(GPIO_PORTD_BASE, GPIO_PIN_6 | GPIO_PIN_7);
//
// Initialize the UART1.
//
//UARTStdioConfig(1, 9600, 16000000);
UARTClockSourceSet(UART2_BASE, UART_CLOCK_PIOSC);
UARTConfigSetExpClk(UART2_BASE, UART_CLOCK_PIOSC ,9600,UART_CONFIG_PAR_ZERO);
UARTFIFOEnable(UART2_BASE);
}
//*****************************************************************************
//
// This function provides a 1 second delay using a simple polling method.
//
//*****************************************************************************
void
SimpleDelay(void)
{
//
// Delay cycles for 1 second
//
SysCtlDelay(16000000 / 3);
}
//*****************************************************************************
//
// Send a string to the UART0.
//
//*****************************************************************************
void
UART1Send(const uint8_t *pui8Buffer, uint32_t ui32Count)
{
//
// Loop while there are more characters to send.
//
while(ui32Count--)
{
//
// Write the next character to the UART.
//
while(!UARTSpaceAvail(UART1_BASE)){
//Wait till space in Tx FIFO is available.
UARTFIFODisable(UART1_BASE);
UARTFIFOEnable(UART1_BASE);
}
UARTCharPut(UART1_BASE, *pui8Buffer++);
//
// Turn on the LED (Green).
//
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3, GPIO_PIN_3);
SimpleDelay();
// Turn off the LED (Green).
//
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3, 0x00);
//
// Turn on the LED (Blue).
//
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, GPIO_PIN_2);
SimpleDelay();
//
// Turn off the LED (Blue).
//
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, 0x00);
}
}
//*****************************************************************************
//
// Configuration for blinking LEDs.
//
//*****************************************************************************
void
ConfigureLED(void){
//
// Enable the GPIO port that is used for the on-board LED.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
//
// Check if the peripheral access is enabled.
//
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOF))
{
}
//
// Enable the GPIO pin for the LED (PF3, PF2, PF1).
// Set the direction as output, and enable the GPIO
// pin for digital function.
//
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_3);
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_2);
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1);
}
//*****************************************************************************
//
// Main Function
//
//*****************************************************************************
int
main(void)
{
ConfigureLED();
ConfigureUART1();
ConfigureUART2();
while(true){
uint32_t rec = 0;
UART1Send((uint8_t *)"ABCDEFGHIJKLMNOP",16);
SimpleDelay();
while(!UARTCharsAvail(UART2_BASE)){
//
// Wait till a character is present in the Receive FIFO of UART2.
//
}
//
// Fetch the character. 'rec' will be true or false depending on the
// presence of character in the receive FIFO.
//
rec = UARTCharGetNonBlocking(UART2_BASE);
if(rec){
//
// Turn on the RED LED.
//
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, GPIO_PIN_1);
SimpleDelay();
//
// Turn off the RED LED.
//
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, 0x00);
SimpleDelay();
}
}
}

: