Part Number: RM57L843
10.4.3 Entering CPU Idle Mode
After enabling the STC test by writing the STC enable key, the test is triggered only after the CPU is taken
to idle mode by executing the CPU Idle Instruction asm(“ WFI”).
10.4.4 Entering nHET Idle Mode
After enabling the STC test by writing the STC enable key, the test is triggered only after the nHET
module is put in reset state by writing to bit 0 the HETGCR Global Configuration Register in the nHET
module.
STC1 segment1 is μSCU. If I want to test μSCU, should I also enter CPU Idle Mode?