Part Number: TM4C1294NCPDT
Tool/software: Code Composer Studio
Hi together,
i want to convert 3 analog inputs over 1 sequencer with the following settings.
When I debug my code, than it look like I have a problem with the FIFO.
With the first Interrupt there were stored 3 values in the “adcBuffer2” variable. And in the next interrupts the adcBuffer2 stored 6 values. I don’t understand why this happened.
Have you any idears?
//
// Library Generals
//
#include "stdbool.h"
#include <stdio.h>
#include <stdint.h>
//
// Library TivaWare
//
#include "driverlib/sysctl.h"
#include "driverlib/interrupt.h"
#include "driverlib/adc.h"
#include "inc/tm4c1294ncpdt.h"
#include "inc/hw_memmap.h"
//
// Library own
//
#include "adc2.h"
//
// Globale Variablen
//
uint32_t adcBuffer2[30];
uint32_t adcGetValues;
//
// Interrupt Handler ADC0SS0
//
void ADC0IntHandler(void) {
uint32_t test = 0;
// Clear interrupt Flag
ADCIntClear(ADC0_BASE, 0);
ADCSequenceDataGet(ADC0_BASE, 0, adcBuffer2);
adcGetValues=1;
}
void main(void) {
adcGetValues=0;
uint32_t sysclock_read=0;
sysclock_read=SysCtlClockFreqSet(SYSCTL_OSC_INT | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480, 120000000);
printf("Systemclock is set to: %d\n", sysclock_read);
// ADC Init
adc2_init();
IntPrioritySet(INT_ADC0SS0, 0x00);
//
// ADC0SS0 Interrupt source
//
ADCIntRegister(ADC0_BASE, 0, ADC0IntHandler);
//
// Register Interrupt to NVIC
//
IntRegister(INT_ADC0SS0, ADC0IntHandler);
//
// ADC0 enable
//
ADCIntEnable(ADC0_BASE, 0);
//
// Interrupt ADC0SS0 enable
//
IntEnable(INT_ADC0SS0);
//
// Enable Global Interrupts
//
IntMasterEnable();
//
// Sequencer enable
//
ADCSequenceEnable(ADC0_BASE, 0);
while(1){
if (adcGetValues==1) {
ADCSequenceDisable(ADC0_BASE, 0);
ADCIntDisable(ADC0_BASE, 0);
IntDisable(INT_ADC0SS0);
//ADCSequenceDisable(ADC0_BASE, 0);
/*
printf("ADC Value1: %d\n", adcBuffer2[0]);
printf("ADC Value2: %d\n", adcBuffer2[1]);
printf("ADC Value3: %d\n", adcBuffer2[2]);
*/
adcGetValues = 0;
ADCIntEnable(ADC0_BASE, 0);
IntEnable(INT_ADC0SS0);
ADCSequenceEnable(ADC0_BASE, 0);
}
}
}
#include <stdint.h>
#include <stdbool.h>
#include <stdio.h>
#include "inc/tm4c1294ncpdt.h"
#include "inc/hw_memmap.h"
#include "driverlib/sysctl.h"
#include "driverlib/adc.h"
#include "driverlib/gpio.h"
#include "driverlib/comp.h"
#include "func.h"
adc2_init(){
uint32_t adcClock=0, adcDiv=0;
//
// Enable the ADC0 peripheral
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0); wait();
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE); wait();
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3);
//
// Configure the ADC to use PLL at 480 MHz with Full rate devided by 30 to get 16 MHz
//
ADCClockConfigSet(ADC0_BASE, ADC_CLOCK_SRC_PLL | ADC_CLOCK_RATE_FULL, 30);
ADCSequenceDisable(ADC0_BASE, 0);
//
// Read the current ADC configuration
//
adcClock=ADCClockConfigGet(ADC0_BASE, &adcDiv);
printf("ADC clock is: 0x%x, div: 0x%x\n", adcClock, adcDiv);
//
// Hardware averageing: by a faktor of 2 -> 2,4,8,16,32,64
//
ADCHardwareOversampleConfigure(ADC0_BASE, 0);
//
// ADC voltage-lvl reference set to intern
//
ADCReferenceSet(ADC0_BASE, ADC_REF_INT);
//
// ADC Sequencer config: Source ADC0, Sequencer 0, Trigger: always, priority: 0
//
ADCSequenceConfigure(ADC0_BASE, 0, ADC_TRIGGER_ALWAYS, 0);
//
// ADC Sequencer step
// 1. Source-ADC -> ADC0_BASE
// 2. Source-Sequencer -> 0
// 3. Sample-Value depends in the depth of the FIFO, by Sequencer 0 it is up to 7 (0-7)
// 4. Config-> select input-channel AINx, interrupt specification
//
ADCSequenceStepConfigure(ADC0_BASE, 0, 0, ADC_CTL_CH0);
ADCSequenceStepConfigure(ADC0_BASE, 0, 1, ADC_CTL_CH1);
ADCSequenceStepConfigure(ADC0_BASE, 0, 2, (ADC_CTL_CH2 | ADC_CTL_IE | ADC_CTL_END));
}