Part Number: EK-TM4C123GXL
Hi,
The MSG_OBJ_DATA_LOST flag is set, but is never cleared by CANMessageGet.
I tried this
but nothing happened.
My code is:
while(1)
{
ROM_CANMessageSet(CAN0_BASE, TXOBJECT, &g_sCAN0TxMessage, MSG_OBJ_TYPE_TX_REMOTE);
delay(50); // wait 100ms
if(g_ui32ErrFlag != 0)
{ // check for errors
//UARTprintf("CAN Bus Error\n");
CANErrorHandler();
}
if(g_bRXFlag)
{ // rx interrupt has occured
g_sCAN0RxMessage.pui8MsgData = msgData; // set pointer to rx buffer
ROM_CANMessageGet(CAN0_BASE, RXOBJECT, &g_sCAN0RxMessage, MSG_OBJ_TYPE_RX); // read CAN message object RXOBJECT from CAN peripheral
g_bRXFlag = 0; // clear rx flag
if(!(g_sCAN0RxMessage.ui32Flags & MSG_OBJ_DATA_LOST))
{
UARTprintf("CAN_ID: 0x%2x\t", g_sCAN0RxMessage.ui32MsgID);
UARTprintf("Data: %02x %02x %02x %02x\n", msgData[3], msgData[2], msgData[1], msgData[0]);
}
else
{
g_sCAN0RxMessage.ui32Flags &= ~MSG_OBJ_DATA_LOST;
ROM_CANMessageGet(CAN0_BASE, RXOBJECT, &g_sCAN0RxMessage, MSG_OBJ_TYPE_RX);
}
}
}
Any hits.
Regards
Andrés