Part Number: EK-TM4C123GXL
Other Parts Discussed in Thread: ENERGIA
Tool/software: TI-RTOS
Hello,
I am working on interfacing multiple sensors to TM4C123G microcontroller and read the data via UART and store it in a buffer and transmit the same via USB interface. I am facing issues in reading the data via UART, it just returns nothing when I try to read and blocks my next statements. Following is a snippet of the code,
Void echoFxn(UArg arg0, UArg arg1)
{
uart_multiple_init();
while(1)
{
//UART_read(uart1, a, sizeof(a));
// UART_read(uart2, c, sizeof(c));
UART_read(uart3, b, sizeof(b));
UART_write(uart3, b, sizeof(b));
}
}
static void uart_multiple_init()
{
//Create a UART with data processing off.
UART_Params_init(&uartParams);
uartParams.writeDataMode = UART_DATA_BINARY;
uartParams.readDataMode = UART_DATA_BINARY;
uartParams.readReturnMode = UART_RETURN_FULL;
uartParams.readEcho = UART_ECHO_OFF;
uartParams.baudRate = 115200;
uart = UART_open(Board_UART0, &uartParams);
if (uart == NULL) {
System_printf("NOT opened");
System_flush();
//Turn on user LED
GPIO_write(Board_LED0, Board_LED_ON);
System_abort("Error opening the UART");
}
UART_Params_init(&uartParams1);
uartParams1.writeDataMode = UART_DATA_BINARY;
uartParams1.readDataMode = UART_DATA_BINARY;
uartParams1.readReturnMode = UART_RETURN_FULL;
uartParams1.readEcho = UART_ECHO_OFF;
uartParams1.baudRate = 115200;
uart1 = UART_open(Board_UART1, &uartParams1);
if (uart1 == NULL) {
System_printf("UART1 NOT OPEN");
System_flush();
// Turn on user LED
GPIO_write(Board_LED0, Board_LED_ON);
System_abort("Error opening the UART");
}
UART_Params_init(&uartParams2);
uartParams2.writeDataMode = UART_DATA_BINARY;
uartParams2.readDataMode = UART_DATA_BINARY;
uartParams2.readReturnMode = UART_RETURN_FULL;
uartParams2.readEcho = UART_ECHO_OFF;
uartParams2.baudRate = 115200;
uart2 = UART_open(Board_UART2, &uartParams2);
if (uart2 == NULL) {
System_printf("UART2 NOT OPEN");
System_flush();
//Turn on user LED
GPIO_write(Board_LED0, Board_LED_ON);
System_abort("Error opening the UART");
}
UART_Params_init(&uartParams3);
uartParams3.writeDataMode = UART_DATA_BINARY;
uartParams3.readDataMode = UART_DATA_BINARY;
uartParams3.readReturnMode = UART_RETURN_FULL;
//uartParams3.readEcho = UART_ECHO_OFF;
uartParams3.baudRate = 115200;
// uartParams.readMode = UART_MODE_CALLBACK;
// uartParams.readCallback = readCallback;
uart3 = UART_open(Board_UART3, &uartParams3);
if (uart3 == NULL) {
System_printf("UART3 NOT OPEN");
System_flush();
//Turn on user LED
GPIO_write(Board_LED0, Board_LED_ON);
System_abort("Error opening the UART");
}
}
I request someone to help me on this, I need atleast one UART to receive the data, so that I can solve other UART receive.